Machine Tools

NSK is the only manufacturer to offer a complete development and supply service for the essential parts required for machine tools. NSK enjoys unshakeable global product strength for its bearings used in machine tools. These include:
- high precision bearings supplied from Japan and the United Kingdom
- spindles that offer easily the fastest spin speed capability available, and are of the highest standard in their class worldwide
- ball screws that have achieved top global brand status as a result of the cutting-edge technologies used
- NSK Linear guides™ that are manufactured using production technologies guaranteeing high precision and product quality.
NSK possesses analytical technologies closely based on tribology (friction control technologies) which are used to reduce energy losses to the absolute minimum, as well as evaluation technologies to rigorously assess how best to meet customer needs, and lubrication technologies that achieve both reductions in energy losses and increases in capacity.
NSK is also continuing to amass key materials engineering technologies that contribute to longer product life. Further, in response to customer requirements for precision bearings for high functionality and environmental protection, the company is developing environmentally friendly products.
As a comprehensive manufacturer of machinery parts, NSK is able to meet the increasingly sophisticated needs of its clients, and it can assist with both a speedy commencement of operations for machine tools, as well as optimal overall operation.
Cutting
Enhanced energy efficiency for your machine tools
As a system supplier, NSK offers linear guides, ball screws and super precision bearings .
During the design stage, our experienced application engineers help you to select the components that will enhance the energy efficiency, accuracy, and speed of your machine tools and thereby will boost your machine productivity.
Linear Guides for Machine Tools
Linear Roller Guide RA Series
In response to the demand for guides with high load capacity, rigidity, high-speed, high-precision, high-quality, as well as to the demand for easy maintenance, rolling guides which have above features are becoming prevalent. In order to meet these requirements, NSK, have developed new Linear Roller Guides and we have been widely accepted for the newest machines. >>
Ball Screws
Nut Cooling Ball Screw
Simplifying Ball Screw cooling to make precision machines faster and more precise. Nut cooling can be implemented (for HMD nuts) without changing the machine design. >>
Bearings for Machine Tools
Super Precision Ball Bearings
Designed to meet the requirements of demanding applications: high accuracy, high rotational speed and high rigidity. These bearings deliver the highest level of accuracy, supported by our production capability, state-of-the-art equipment and extensive manufacturing expertise >>
BSBD Series Ball Screw Support Bearing
Ball Screw Support bearings - designed to be compact, ready for easy & accurate installation, greased for life, with low friction and heat generation sealing. >>
Milling machines
Optimum machining quality even at higher speeds
High speeds, multi-shift or start/stop operations, high level of abrasive contamination use of coolants and lubricants, and a wide range of materials – NSK’s high-precision products excel by delivering unsurpassed finishing accuracy, even in these conditions. They enable ultra-high speeds, work extremely reliable and precise and are also quiet, meaning they tick all the boxes for optimum machining quality and cost-efficient solutions.
NSK’s patented new materials and components, extremely wear-resistant, further improve the performance of your machines.

Bearings for Machine Tools
Angular Contact Ball Bearings with SURSAVE Cage - Ultra-High Speed
The ROBUST range is primarily used for high speed applications, where robustness is required. With the medium ball size, the option of direct lubrication through the outer ring, our “Sursave” cage and the option for SHX steel, we have the right solution for your individual application >>
Ball Screws
Nut Cooling Ball Screw
There are several sound arguments for maintaining a stable temperature below 40°C in ball screws to guarantee the utmost precision. This is because the fast motion of the nut raises the operating temperature and thereby prompts changes in running behaviour. A temperature increase of just 10°C causes a 1-metre-long spindle to stretch by 120 µm, which means that the machine tool can no longer deliver the necessary precision. Our specially developed nut cooling system drastically reduces heat generation, enabling consistent machining results. This means the necessary operating temperature can be maintained >>
Grinding machines
Zero tolerance for contamination
Modern grinding machines such as cylindrical, surface, tool and jig grinding machines are used to process a wide range of work pieces. They have to maintain very precise tolerances and roughness values. Over time, the lubricants and coolants used become contaminated. This causes severe abrasive wear to the machine’s components.
Compact, robust ball screws from the BSS series together with NSK’s innovative X1 seal concept ensure low-friction movements and high speed sealed ACBB make sure, that grinding machines run reliably. As a result, servicing intervals can be substantially extended, reducing maintenance costs.

Ball Screws
Lathes
Zero tolerance for contamination
Reliable, high-precision motion products are needed for lathes turning machines to achieve the highest possible material throughput without downtime.
The high rigidity and load rating of NSK’s linear guides and precision bearings pave the way for a long service life, leading to enhanced productivity for your turning machines.

Ball Screws
Electrical Discharge Machining (EDM/EWM)
Improved precision and safety
Electrical discharge machines for high-precision applications require highly accurate mechanical components. NSK’s ball screws and the support bearings as well as the linear guides help to make the spark erosion process safe and are also ideal for high traverse rates. With their compact design, they are perfect for delivering precision in confined spaces.

Linear Guides
Linear Roller Guide RA Series
Ultra-high load ratings, unique rigidity.
As the latest generation of roller guides, NSK’s RA series delivers outstanding motion accuracy. This is achieved by means of large rolling elements, ultra-high load ratings and rigidity. Meanwhile, the patented K1 lubrication unit enables long maintenance-free operation. Roller guides from the RA series also feature very low levels of vibration thanks to their specially constructed retaining and diverting components. This prevents the rollers from skewing >>
Demands for increasingly efficient energy conversion are leading to electromechanical drive concepts in various branches of industry. The process of metal manipulation – i.e., stamping, forming, and bending – has a major impact on how mechanical components are designed.
Linear guides, ball screws and bearings are replacing hydraulic drive solutions because they mobilise power reserves and help to significantly reduce driving axles. NSK’s cooled ball screws also increase the amount of heat which is transferred.
Typical machines using our products are Laser machines, bending, press brake, presses or punching.

Linear Guides
Linear Guides - NH and NS Series
Linear guides from the NH and NS series offer maximum precision combined with extremely high load ratings. Outstanding accuracy means that the object in motion is positioned precisely and moves optimally. It also guarantees smooth, even running >>
Ball Screws
Ball Screws - HTF-Series
The HTF-Series offers several types of Ball Screws for high-speed, high-load applications. >>
Bearings
BSBD Series Ball Screw Support Bearing
Ball Screw Support bearings - designed to be compact, ready for easy & accurate installation, greased for life, with low friction and heat generation sealing. >>
TAC-Series Thrust Angular Contact Ball Bearings for Ball Screw Support
The NSKHPS TAC-series of Support Bearings for Ball Screws is available with a product lineup, as the bearings were improved by focusing on material cleanliness. >>
NSK TAC-03 Series Ball Screw Support Bearings for High Load Application
The series allow users to maintain high capacity performance with a smaller diameter of the screw shaft end. >>
Spindles
Enhanced energy efficiency for your machine tools
Spindles are at the heart of every machine and the bearing is the heart of the spindle. Therefore, the spindle manufacturer has to rely on the bearing’s quality and performance.
Bearings
ROBUST Series - Angular Contact Ball Bearings
The best option for main spindles in machine tools that require ultra-high speeds >>
SHX Steel
SHX is a heat-resistant & wear resistant steel resulting from NSK’s special proprietary materials & heat treatment technology; it offers unrivalled ultra high-speed performance and extended fatigue life ideally suited for machine tools running to their maximum capacity >>
Oil-Air Lubrication for Super Precision Bearings
NSK's oil-air lubrication works as a safe, economic and pollution free lubrication. With a lubricating hole (groove and hole in the outer ring) the lubricant quantity can be controlled and is injected precisely into the bearing, even under high speed. In addition this reduces the number of parts in the bearing and so simplifies the overall possible construction of the spindle >>
Driven
Sealed Angular Contact Ball Bearings are often required for driving tool applications. NSK ACBB are supplied with lifelong lubrication to ensure that no maintenance is needed – something which is essential in this context.

Bearings
Angular Contact Ball Bearings - Sealed ACBB
NSK's Sealed Angular Contact Ball Bearings ensure that the bearings are in the best possible condition, free of contamination, before and during operation while providing high level machining performance >>
Tool turrets
Bearings have to withstand loads as well as high temperatures, multi-shift operation or start-stop operation. NSK’s angular-contact ball bearings are the ideal solution for machine tool turrets.
Total Quality Solution:
Standard spindle bearings, NSKHPS Angular-contact ball bearings, Tapered roller bearings, and Cylindrical roller bearings.


NSK Launched ACOUS NAVI™ Condition Monitoring & Diagnostic Software for FIELD System
ACOUS NAVI is a complete solution designed to monitor the operating status of machine components and detect or predict signs of damage or deterioration. It is provided to customers as an application that can be installed on a PC or as a pre-installed solution on dedicated hardware.
The ACOUS NAVI line-up includes three main versions to monitor and diagnose the status of bearings, ball screws, and linear guides.
Share