Descarga de la aplicación EDD Megaterm
About EDD Megaterm
The EDD Megaterm application supports the setting and editing of parameters and configurations for EDD Drive Units. This software is for use on PC and is provided free of charge.
Note: The software can be used only with EDD Drive Units.
After agreeing to the license agreement on the following page, you may proceed with downloading the software and Instruction Manual.
Category | Name | File Type | File Size | Ver. (Release Date) |
---|---|---|---|---|
Software | EDD Megaterm Windows 7 (32-bit) | ZIP | 7.43 MB | 1.2.2.0 (2023/03/03) |
Software | EDD Megaterm Windows 7 (64-bit) | ZIP | 7.44 MB | 1.2.2.0 (2023/03/03) |
Software | EDD Megaterm Windows 10 (32-bit) | ZIP | 7.43 MB | 1.2.2.0 (2023/03/03) |
Software | EDD Megaterm Windows 10 (64-bit) | ZIP | 7.44 MB | 1.2.2.0 (2023/03/03) |
Megaterm Application Software Operation Environment:
OS*1 | Windows 7 Home/Professional/Enterprise/Ultimate Windows 10 Home/Pro/Enterprise *1 With Internet Explorer 11 or above |
---|---|
CPU | 1 GHz or above 32-bit (x86) or 64-bit (x64) CPU |
Memory | 1 GB or above (32-bit) or 2 GB or above (64-bit) |
HDD | 16 GB (32-bit) or 20 GB (64-bit) or more free space available |
Display | 800 × 600 (SVGA) or above |
Ports | USB |
With the following system fonts:
- Courier New, Arial
Installing EDD Megaterm
1. WinUSB
Run WinUSB from [\Install\WinUSB\WinUSB.vbs] and install device drivers.
2. EDD Megaterm
Run setup from [\Install\EDDmegaterm\setup.exe] and install the Megaterm application.
How to Use EDD Megaterm
After installation completes, please see “Online Help.”
Notes:
- Company and product names listed are registered trademarks of their respective companies.
- The reproduction, copy, or alteration of information contained within without permission from NSK Ltd. is prohibited.
- The information contained within is subject to change without advance notice.
NSK Program License Agreement
This “Program” is copyrighted by NSK Ltd. (hereinafter NSK) and is not for sale; it is licensed for use. Under the terms of this License Agreement, NSK grants the user usage rights to the “Program” in the country where downloaded (hereinafter the “Usage Agreement”). NSK assumes no responsibility for the installation, usage, or results of the “Program” or that these will meet user expectations.
1. Usage Rights
Use of the “Program”
For each download of the “Program”, the user may (1) use the “Program” on one machine, or (2) transfer the “Program” to a third party.
If the “Program” is transferred to a third party, this “NSK Program License Agreement” must also be transferred. The user may transfer the program to a third party provided that the transferee agrees to the “NSK Program License Agreement.” Once a third party has agreed to the agreement, the original user’s usage rights will end.
The user must NOT (1) transfer or use the “Program” in any way not specified by this License Agreement; (2) transmit the “Program” by e-mail, etc.; (3) duplicate, change, combine, or distribute the “Program”; (4) decompile, disassemble, reverse engineer, or adapt the “Program”; or (5) relicense, lease, or loan the “Program.”
2. Copyright
In all cases, the copyright for this software, documentation, etc. belongs to NSK.
3. Warranty
This program is provided as is with no warranty of any kind.
No program services such as upgrades, etc. will be provided.
The warranty specified above for the “Program” is in lieu of all other warranties, express or implied, and including those statutory warranties against defects, for merchantability, or of fitness for purpose.
4. Limitation of Liability
NSK is not liable for lost profits, indirect damages, extended damages, or damages that occur for extraordinary reasons, either foreseen or unforeseen.
NSK is not liable for claims for damage from a third party. The above Limitation of Liability also applies to claims for damage/loss against the “Program” developer who supplied the “Program” to NSK.
5. Other
The user may terminate this Usage Agreement at any time without notifying NSK. In this case, the user’s usage rights for the “Program” will be terminated.
NSK may also terminate this contract if the user violates this Usage Agreement. In this case, the usage rights for the program will be revoked, and the user must delete, destroy, or otherwise make unusable any copies of the software they possess.
EDD Megaterm Application Download
Please download the appropriate file below and install the application.
If you are already using the EDD Megaterm, please uninstall the EDD Megaterm you are using and then reinstall the latest version.
Category | Name | File Type | File Size | Ver. (Release Date) |
---|---|---|---|---|
Software | EDD Megaterm Windows 7 (32-bit) | ZIP | 7.43 MB | 1.2.2.0 (2023/03/03) |
Software | EDD Megaterm Windows 7 (64-bit) | ZIP | 7.44 MB | 1.2.2.0 (2023/03/03) |
Software | EDD Megaterm Windows 10 (32-bit) | ZIP | 7.43 MB | 1.2.2.0 (2023/03/03) |
Software | EDD Megaterm Windows 10 (64-bit) | ZIP | 7.44 MB | 1.2.2.0 (2023/03/03) |
Compartir