Tokyo, Japan, March 5, 2010 - NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) announced today that it has developed a nut cooling ball screw that has a cooling mechanism in the nut, a feature that was designed to accommodate the increasing speed and precision of machine tools. NSK will launch this product in May 2010 and plans to expand the lineup in the future. It expects annual sales to reach 1 billion yen by 2012.
NSK started marketing hollow shaft ball screws, which are cooled by a coolant flowing through the screws' hollow shafts, in the 1980s. This sort of ball screw has accommodated the development of higher speed and greater precision in machine tools. In recent years, the feeding speed of objects to process on machine tools has been increased even further in order to boost productivity, especially in the processing of automotive and aircraft parts. Also, the precision of machine tools for die machining and microfabrication has improved. Consequentially, there is demand to reduce temperature variation in the entire machine, not just the screw shaft, in order to prevent adverse effects on precision. At the same time, demand for large products such as windmill equipment and rolling stock has increased greatly, and the speed of large machine tools has increased as a result.
The need has therefore increased for a new cooling system that is inexpensive, simple, compact, and that improves the cooling function in order to facilitate the increasing speed and precision of machine tools.