Tokyo, Japan, January 26, 2010 - NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) announced that it has developed an ultra-low friction roller clutch* for fishing bait reels that reduces overrunning friction by 90% compared to conventional roller clutches, to enhance reel operation and reeling feel. The company targets annual sales of 100 million yen for this product by 2012.
* Roller clutch: Used to prevent reverse rotation during reeling. The roller clutch overruns during reeling. When there is a tug on the line, the rollers drop onto the wedged face of the outer raceway to securely lock the roller clutch in one direction only.