Tokyo, Japan, November 5, 2013 – NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) will exhibit at the International Robot Exhibition 2013,which is to be held at Tokyo Big Sight (Ariake, Koto-ku, Tokyo) from Wednesday, November 6 through Saturday, November 9, 2013.
The purpose of NSK attending this expo is to interact with related companies towards the mutual target of advancing robotic technology and to get feedback from many visitors. NSK is searching for new needs and seeds in the market pertaining to robot and sensor technology.
NSK is a participant in the Kanagawa Sagami Robot Industry Special Ward Robot Demonstration Support Business. The company will be exhibiting at its own booth and at the Kanagawa Pavilion.
| Robots |
Obstacle Avoidance Guide Robots (first time to display this technology) |
| Portable Guide Robot with Automatic Obstacle Avoidance (first time to display this technology) |
| Sensor Technology |
Optical Kinesthetic Sensors (first time to display this technology) |
| Compact, High-Resolution Encoder Unit (first time to display this technology) |
| Proximity Sensor Technology*1 |
- (1) Obstacle Avoidance Guide Robot
- This product makes it possible for first-time visitors to arrive at their destination within a hospital or office building without getting lost. The user simply selects a preregistered destination and then the robot uses map and
- (2) Optical Kinesthetic Sensor
- Compared to the conventional strain gauge sensor, the optical sensor that NSK developed is non-contact and therefore does not break easily. It is also not very susceptible to temperature. NSK envisions its kinesthetic sensors to be used for the input interface of obstacle avoidance guide robots and other applications such as that of detecting the kinesthetic sense of industrial robots used in manufacturing lines.
- (3) Compact, High-Resolution Encoder Unit
- This sensor uses the polarizing-axis detection method and, compared to the conventional optical transmission sensors (minimum outer diameter 5 to 6 mm; 1,000 to 2000 pulses/revolution), it has a compact outer diameter of 6 mm and a highly precise level of detection, at 16,384 pulses per revolution. NSK envisions that its compact, high-resolution encoder unit will be used in the small joints of robots as well as precision measurement instruments and semiconductor manufacturing equipment.
- (4) Proximity Sensor
- This kind of sensor works by emitting LED light and then confirming the presence of objects and the distance to any such object by the light that is reflected back.Multiple elements are arranged in linear fashion to obtain the distance to objects and the center position thereof in real time.
NSK developed this technology for application to obstacle avoidance for human-assistance robots. The major benefit of this sensor is that it can obtain multiple sensor element information with little wiring for a detection speed that achieves a response time of 1 millisecond or faster, eliminating the need for emergency avoidance operations. In addition, NSK has used soft material for the mounting board to provide flexibility. NSK will provide a demo of this technology at the expo.