Tokyo, Japan, October 17, 2014 - NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) today announced that it has developed a super long-life planetary shaft for use in planetary mechanisms* used in automobile automatic transmissions (AT), continuously variable transmissions (CVT), hybrid systems, etc.
NSK optimized the heat treatment process and materials in order to lengthen the life of the type of planetary shafts that are staked at both ends. As a result, the overall planetary mechanism can be smaller and lighter, contributing to improved fuel in automobiles.
NSK is targeting 2 billion yen in global sales for this product in 2018.
*Planetary mechanism: | A mechanism that accelerates, decelerates and reverses the rotational force input from the engine by using a combination of the rotation and revolution of multiple gears. |