Press Release

NSK welcomes visitors to the 49th Pulp & Paper International Exhibition

The NSK Brazil will be at 49th Pulp and Paper International Exhibition, held by ABTCP - Brazilian Pulp and Paper Technical Association, which happens from 25th to 27th October, at Expo Center Norte, in Sao Paulo. The company will exhibit products developed for this segment, as spherical roller bearings - TL and NSKHPS™ series, and the AIP - Asset Improvement Program.

Based on a standard methodology, the AIP program aims are saving costs and increasing the productivity of NSK customers.

“The AIP is a worldwide successful program, due to show it is possible to raise the bearing durability and the performance, therefore the company gets cost saving and more efficient process”, says Luiz Granjo, Strategic Planning & Marketing manager from NSK Brazil.

booth image

NSKHPS High Performance Standard Bearings for Industrial Machinery

NSKHPS High Performance Standard Bearings for Industrial Machinery

NSK successfully developed the NSKHPS series of spherical roller bearings, which provide a longer service life and higher limiting speeds, by employing leading-edge materials and technology in combination with years of cultivated experience and technical know-how.
Features:
  1. Bearing life increased by twofold (increased dynamic load rating by 25%).
  2. Limiting speed increased by 20%.

TL Series Spherical Roller Bearings

Provide superior resistance to inner ring fractures, which is ideal for papermaking machinery operating under high-temperature conditions. The tough, long-life, TL series of bearings help boost productivity and lower costs.

Features:
  1. Adopting NSK's proprietary steel grade (new specification bearing material) and a special case hardening and heat treatment process, resistance against inner ring fracturing has been dramatically improved.
  2. Raceway surface hardness has been increased for longer life performance.
  3. Dimensional stability under high temperature (200℃) operating conditions.

Overview of Exhibition

Name of Exhibition 49th Pulp and Paper International Exhibition
Location Expo Center Norte - Sao Paulo
Dates From Tuesday, 25th to Thursday, 27th October, 2016
From 1 pm to 8 pm
NSK Booth No. Booth 44 and 45 on 129 street B
Official website http://www.abtcp2016.org.br/en/ New Window