Press Release

NSK Welcomes Visitors to VANZ 2017

NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Toshihiro Uchiyama) announced that it will exhibit its products and technologies at VANZ 2017, to be held at Novotel Rotorua Lakeside (Rotorua, New Zealand) from May 16 to May 18, 2017.

Summary of the Exhibition

VANZ (Vibrations Association of New Zealand) is an association formed as a focus group on reliability engineering principles. The association has strong support from the leading manufacturing, engineering and infrastructure business throughout New Zealand and Australia where the exchange of technologies and ideas is facilitated. This event is a conference run by the association, at which key CEO, Managing Directors and key business representatives, along with the top reliability focused engineers such as those from Fonterra attend.

NSK as a manufacturer provides an exhibit for the delegates to come and discuss their problematic issues. NSK will exhibit key solution products such as NSKHPS, Molded-OilTM and ES1 Stainless Steel bearings. NSK will be presenting an insight into bearing failure analysis, and how understanding this, can improve reliability.

Booth Image
Booth Image

Major Exhibits

1. NSKHPS™ series
NSKHPS High Performance Standard Bearings for Industrial Machinery are contributes lower maintenance costs and supports downsizing by the high performance.
NSKHPS series
2. Molded-Oil™
Molded-Oil Bearings are provided with ample lubrication for extended periods from oil seeping with a polyolefin resin for excellent performance in water and dust contaminated environments.
Molded-Oil
3. Stainless Steel Bearings ES1 series
Stainless steel bearings, the standard products of the NSK SPACEA™ Series for special environments, are suitable for high-humidity environments.
Stainless Steel Bearings ES1 series

Overview of Exhibition

Name of Exhibition VANZ 2017
Organizer Vibrations Association of New Zealand
Date May Tuesday 16 to May Thursday 18, 2017
8:30 a.m. - 5:00 p.m.
Venue Novotel Rotorua Lakeside (Rotorua, New Zealand)
NSK Booth No. #11
Official Website http://vanz.org.nz/ New Window