Press Release

NSK Develops Lift-Rotation Z-θ Actuator Unit

Compact design fits inside vertical machine tools and injection molding machinery. Increase productivity per square meter of floor space.

NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President & CEO: Toshihiro Uchiyama) has developed a new actuator unit that delivers lift-rotation Z-θ motion (coaxial rotation and linear motion) in a compact rod-shaped package.

The versatile unit uniquely integrates motor, ball screw with spline, and brake mechanism to achieve high performance Z-θ motion with a small footprint. A waterproof upper structure enables the unit to handle challenging splash-and-spray (wet) manufacturing environments.

NSK will be exhibiting a working prototype at International Robot Exhibition 2019 (iREX 2019), to be held at Tokyo Big Site from December 18-21, 2019.

The Z-θ actuator offers a new value proposal of increasing productivity per square meter of floor space. NSK is preparing to launch the product in the near future, and units are available for trial implementation and verification testing by customers.

Development Background

There is a recent trend toward downscaling manufacturing procedures, a process which is measured by calculating productivity on a plant floor space (per-square-meter) basis. Downscaling of machinery is taking shape through compact vertical machining centers and vertical injection molding machines, with many such machines recently hitting the market.

General manufacturing automation employs robots to transfer and convey workpieces (product) between manufacturing processes. SCARA robots are often used for pick-and-place transfer tasks, but are limited by nature of their design in that they cannot place items near their own arm support base. This results in SCARA robots taking up significantly more floor space than necessary, thereby reducing productivity on a plant floor space (per-square-meter) basis.

The newly developed lift-rotation Z-θ actuator unit delivers coaxial rotation, linear motion, motor, and brake mechanism in a small rod-shaped package with a waterproof upper structure. The compact design of the Z-θ actuator makes it easy to integrate directly inside vertical machining centers and injection molding machines.

Features

  • Combination of direct drive motor and linear motion technology achieves lift-rotation Z-θ motion (coaxial rotation and linear motion) in a compact rod-shaped package.
  • High-speed high-accuracy positioning through combination of NSK Megatorque Motor™ and ROBOTTE™ technology (gearless/beltless structure).
  • O-shaped (hollow) Megatorque Motor enables highly compact rod-shaped unit design.
  • Integrated brake mechanism prevents shaft from dropping under its own weight.
  • Integrated absolute position sensor.
  • The upper section of the unit is waterproof, making it ideal for use in splash-and-spray (wet) manufacturing environments.
Features
Features

Reference Specification

Z Axis Stroke 50mm
Outer Diameter φ150mm
Maximum Motor Torque θ axis:18Nm , Z axis:12Nm

About NSK

NSK started its journey manufacturing the first bearings in Japan in 1916, and has since developed into a global organization researching, designing, and manufacturing Motion & Control™ solutions supporting essential mobility and industry applications. NSK is currently the top supplier of bearings in Japan, and is the third largest supplier in the world by market share.

Our responsive products and technologies are used to enhance automotive performance and industrial productivity while reducing energy consumption to unprecedented low levels.

In the early 1960s we set our sights outside Japan, and to date, have established over 200 business locations across 30 countries.

NSK contributes to a safer, smoother society and helps protect the global environment through its innovative technology integrating Motion & Control. As a truly international enterprise, we are working across national boundaries to improve relationships between people throughout the world.