Press Release

NSK Develops “NSK Feed Drive Adjuster™”

  • NSK Feed Drive Adjuster enables advanced automation of machine tools and reduces environmental impact

NSK announced today that it has developed the NSK Feed Drive Adjuster, a ball screw feed drive accessory that benefits performance and ease of handling and automation of feed drives in machine tools and other production equipment.

The NSK Feed Drive Adjuster will be exhibited at the 31st Japan International Machine Tool Fair (JIMTOF 2022) to be held from November 8-13, 2022. NSK will continue to develop and propose new solutions toward supporting the future of machine tools.


NSK Feed Drive Adjuster

Background

In the field of manufacturing, where a variety of production equipment is used, efforts are underway to realize a sustainable society that is carbon neutral and zero-emission oriented, as well as highly automated and autonomous through the use of big data, backed by the emergence of digital technology.

In order to improve machining accuracy and productivity, machine tools such as machining centers have long been subjected to various design measures and on-site adjustments by skilled technicians to reduce the effects of machine deformation. In recent years, machine tool builders are improving ease of operation and reducing the necessity for specialized technical and skilled labor through the use of rapidly evolving digital technology and data.

Features

The NSK Feed Drive Adjuster minimizes variation (deterioration) in machining performance caused by elongation of the ball screw shaft due to temperature rise in the machine tool feed drive system.

Normally, when the elongation of a screw shaft is significant, it is addressed by releasing axial displacement on one side of the mechanism supporting the screw shaft in order to prevent abnormalities or failure in the feed drive system. However, this reduces ability to bear axial loads and prevents the machine tool from maintaining effective support rigidity (stiffness), affecting the accuracy and quality of machining.


Features

Features

To address this issue, NSK developed the NSK Feed Drive Adjuster to maintain rigidity (stiffness) and dynamic characteristics in the support bearings on one side, while tracking axial displacement. This minimizes changes in rigidity (stiffness) even when the feed drive system is affected by environmental or operational factors, such as heat generation, and maintains the ability to effectively support axial loads, thereby reducing variation (deterioration) in machining accuracy, quality, and productivity.


Features

Benefits

By applying the NSK Feed Drive Adjuster technology to ball screw feed drive systems, the following effects can be expected.

  • Continuously maintaining the rigidity (stiffness) of the ball screw feed drive system improves machining accuracy, quality, and productivity.
  • Enables designing high performance ball screw feed drive system supports without specialized knowledge.
  • Eliminates need for specialized technical skills in fine-tuning control equipment and changing feed rates to match changes in machining conditions.
  • Reduces lost time and environmental impact by reducing or eliminating the need for machine warm-up routines and additional cooling procedures.
  • Realizes optimized coordination of ball screw feed drive system and numerical control system
  • Further improves controllability when combined with NSK ball screws.

In addition, the NSK Feed Drive Adjuster can be used even without electricity (or any energy supply), and can be installed on existing machine tools, contributing to standardization of designs for advanced automation and reduction of environmental impact.

About NSK

NSK began its journey manufacturing the first bearings in Japan in 1916, and has since developed into a global organization researching, designing, and manufacturing Motion & Control™ solutions essential for mobility and industrial applications. NSK is the top supplier of bearings in Japan and is the third largest supplier in the world by market share.

Our responsive products and technologies enhance automotive performance and industrial productivity while reducing energy consumption to unprecedented low levels. In the early 1960s, we set our sights outside Japan and have established over 200 business locations in 30 countries alongside a vast network of joint ventures and partnerships in all corners of the world.

NSK Corporate Philosophy

NSK contributes to a safer, smoother society and helps protect the global environment through its innovative technology integrating Motion & Control. As a truly international enterprise, we are working across national boundaries to improve relationships between people throughout the world.