- NSK rolling bearing data (technical specification, etc.) has been adopted in KISSsoft® and MESYS, two leading design and calculation programs for machinery design
- Having NSK's bearing data built-in by default speeds-up design process and improves convenience for engineers
NSK will begin providing bearing data to MESYS and KISSsoft®, two companies that develop technical calculation software for engineers engaged in machinery design. With this development, engineers will be able to easily and quickly analyze NSK bearings, thereby reducing the time required for bearing selection.

NSK sells rolling bearings worldwide through its branches and distributors in more than 30 countries. In response to requests from mechanical engineers, NSK rolling bearings are now included in the technical calculation software of KISSsoft® and MESYS, both of which are used worldwide, with data available from 2023. The ability to select NSK rolling bearings in both companies' technical calculation software will enhance convenience and customer satisfaction.
The data provided can be updated to provide the latest technical calculations. The data provided at this time covers five bearing types: deep groove ball bearings, angular contact ball bearings, cylindrical roller bearings, tapered roller bearings, and spherical roller bearings, but data for other types of rolling bearings will also be provided in the future.