NSK Ltd.
Corporate Communications Department
NSK Releases Highly Reliable Spherical Roller Bearings for Wind Turbine Main Shafts
Improved wear resistance delivers stable operation with less maintenance over long periods
- A NSK-first combination of bearing material, roller coating, and extra-capacity cage for reducing wear
- A total solution for higher durability—Over 90% less raceway wear compared to standard products
NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Akitoshi Ichii) has developed and launched a line of highly reliable spherical roller bearings (SRBs)1 for wind turbine main shafts that combine three advanced technologies to deliver exceptional reliability. Joining NSK’s “Super-TF” long-life material and high-hardness diamond-like DLC coating, a new extra-capacity ECA cage provides high load capacity in a total bearing solution optimized for the challenges facing today’s wind turbines.
By the full application of these technological advancements, NSK has reduced raceway wear to less than one-tenth that of standard products. As raceway wear is the main form of damage in SRBs for main shafts, this provides a substantial improvement in bearing durability. With fewer maintenance runs and less need to replace parts, these highly reliable bearings help reduce downtime and maintain stable operation at wind power generation facilities worldwide.
NSK has been serving the wind turbine industry with our Super-TF material and DLC coating for years. In June 2024, we developed a SRB with a new extra-capacity ECA cage to serve the needs of wind power companies in North America. Now, we have fully implemented a production system for highly reliable SRBs combining all three of these advanced technologies and we are now expanding fulfillment worldwide.
Future plans involve combining these SRBs with NSK condition monitoring solutions to expand business in maintenance, repair, and operations (MRO). NSK high-reliability spherical roller bearings join a portfolio of aftermarket offerings laid out in our 2026 Mid-Term Management Plan, with a target of 25 billion yen in increased sales in the sector over fiscal 2021.
1 Spherical roller bearings feature an inner ring with two rows of barrel-shaped rollers in contact with a spherical raceway in the outer ring. This configuration supports large loads and gives SRBs self-alignment properties to respond to deflection of the shaft or housing.

Solutions for Wind Turbines: Main Shaft Bearings
1. Development Background
Any component failure in a wind turbine leads to expensive repair costs and extensive downtime. As wind turbines are installed in special environments, such as on mountains and offshore, parts replacement work and the procurement of parts, repair cranes, and other equipment to address damage can take substantial time and resources. Many large parts for wind turbines are made-to-order, and bearings for the main shaft are among the largest components used in machinery. Damage to these crucial parts can result in replacement work that requires about one year or more of downtime2. Therefore, bearings for wind turbine main shafts must be built to last—with high reliability and resistance to premature damage.
Bearings in the main shafts of wind turbines must support the heavy weight of the blades (vanes) and fluctuating loads from changing wind conditions. Spherical roller bearings are the solution of choice, with high load capacity and their ability to tolerate mounting errors and automatically correct for deflection of the shaft or housing (self-alignment). Heavier-than-expected loads under severe operating conditions are the main culprit behind premature damage in SRBs. These factors prevent the necessary oil film from forming in the area between the rollers and bearing rings. Without this lubrication, wear occurs, requiring the bearing be replaced earlier than expected. Thus, improving the wear resistance of raceway surfaces is crucial for turbine uptime and operational reliability.
2 Source: 平成29 年度 電気施設等の保安規制の合理化検討に係る調査風力発電業界の構造調査 [Final Report on FY2017 Structural Study on the Streamlining of Safety Regulations for Electrical Facilities in the Wind Power Generation Industry], Deloitte Tohmatsu Consulting Co. Ltd. 2018.
2. Benefits & Features
1) Improved wear resistance
High-reliability spherical roller bearings for wind turbine main shafts reduce raceway wear by 90% or more compared to standard products. As raceway wear is the main form of damage in these SRBs, NSK’s high-reliability solution boasts significantly improved bearing durability.

Comparison of Raceway Wear
2) Application
Stable turbine operation for extended periods—High-reliability spherical roller bearings extend maintenance intervals and reduce unexpected replacement downtime.
3 .Product Technologies
NSK core technologies in materials, tribology, and analysis combine to provide exceptional resistance to raceway wear. In an NSK first, Super-TF material, a DLC coating, and a high-load capacity cage are combined in a single bearing product.

① “Super-TF” Long-Life Material
NSK-exclusive Super-TF material provides long life by improving surface strength through the uniform distribution of fine carbides throughout. Using Super-TF for the outer and inner rings provides a robust foundation of improved resistance to raceway wear.
② High-Hardness DLC Coating
Diamond-like carbon (DLC) is a generic term for a carbon material that provides unique tribological properties from its mixed composition of graphite and diamond bond structures. Drawing on our expertise in tribology, our high-hardness DLC coating is applied to the rollers to help prevent deterioration of their surface properties. This improves wear resistance where the rollers contact the raceway.
③ New Extra-Capacity ECA Cage
Our newly developed ECA cage is designed to eliminate the need for a guide ring, allowing for a higher quantity of larger rollers. Optimized by NSK’s analysis capabilities, ECA cages boost bearing load capacity while further improving raceway wear resistance.
About NSK
NSK produced the first bearings in Japan in 1916 and over the past 100 years, it has supported the development of industries worldwide by creating various innovative products and technologies in bearings, automotive parts, and precision machinery. Since the early 1960s, the company has expanded overseas and now has operations in about 30 countries. It ranks third in the world in the field of bearings and leads the world in ball screws, electric power steering, and other products.