======================================================================== Before using the application software EDC Megaterm 2006/03 NSK Ltd. ======================================================================== Thank you for using our product. Please read the following notes carefully before using this software. 1.System requirements It is strongly recommended to use EDC Megaterm with the following system. OS Microsoft Windows2000, WindowsXP Software required: Internet Explorer 5.5 or later Fonts required: Courier New, Arial CPU Intel Pentium ‡V 500MHz or faster Memory At least 128MB (256MB or more is recommended for WindowsXP) HDD (Hard disk drive) At least 30MB Display resolution 800~600iSVGAjor higher Hardware At least one RS-232C port or USB port must be available. You can communicate with the EDC driver unit system by using USB to RS-232C converter. Operation confirmed with SRC06-USB(Made by Arvel) RS-232C communication cable is available from NSK as an option. (Type: M-C003RS03) A general-purpose RS-232C communication cable cannot be used because pin assignments are different. In this case, please change cable pin assign according to the user's manual 2.Installation Execute setup.exe to install EDC Megaterm 3.Instructions for use Please refer to the help after the installation is complete. ---------------------------------------------------------------------------- Note: 1. Company and product names mentioned in this document are registered trademarks of each company. 2. It is prohibited to copy, transfer or change the contents of this document without our permission. 3. The contents of this document are subject to change without notice.