Mood, Press, News

Bearings - 25/10/2021

NSK spherical roller bearings with TL technology

NSK TL series spherical roller bearings are active across the world in a host of papermaking machinery applications. Set against conventional spherical roller bearings with standard heat treatment, this advanced product is proving increasingly popular due to a number of distinct benefits that include enhanced inner ring strength, longer service life and dimensional stability at high operating temperatures.

The original development of TL (tough and long life) bearings was to solve a specific problem: inner ring fractures of spherical roller bearings with tapered bores, particularly when used with a relatively high interference fit. This issue can occur on dryer cylinders (including Yankee dryer rolls) and calender rolls, where super-heated steam passes through the hollow journals of dryer rollers and the centre of bearings. The subsequent temperature difference increases the interference fit, producing a tremendous increase in hoop stress (circumferential force) on the inner ring that enhances the potential for cracks.

NSK knew the key to providing a successful solution hinged on the development of a bearing that could better withstand hoop stress. The company therefore set about creating the TL specification based on a steel with a formulation for case-carburising, but using a special method of heat treatment. From a metallurgical standpoint, the raceways are harder than conventional bearing steel but the core remains soft. This contrast delivers the shock resistance needed to prevent fracturing, as well as the necessary surface hardness for long bearing life.


Benchmark tests

The resistance of inner rings that meet the TL specification is higher than the resistance of inner rings made from bainitic steel or standard bearing steel, as demonstrated in a series of benchmark fracture tests. The tests involved subjecting inner rings to a radial load of 2000 kg at a rotational speed of 1800 rpm, while simultaneously applying a measured hoop stress value.

Notably, the rings made from bearing steel, some with standard heat treatment and others with bainite treatment, fractured under hoop stress of 400 MPa after 1 x 107 revolutions and 7 x 107 revolutions respectively (on average). In contrast, the TL specification steel did not fracture under hoop stress of 430 MPa, even after 3 x 108 revolutions (Image 2). The TL rings also marginally outperformed those made from carburised steel with dimension stabilising treatment.

Part of the reason for this high performance was the residual stress (after heat treatment) present in the crack-tested inner rings made from TL specification steel. Residual stress was notably higher in TL steel test pieces in comparison with those made from bearing steel featuring either standard heat treatment or bainite treatment. Residual stress works in the opposite direction to hoop stress, serving to supress this unwanted force.

In fatigue life tests, the TL series bearing all demonstrated far superior performance against the other bearing material types when comparing Weibull plots of the test results (Image 3).

Another significant characteristic of the TL specification is higher surface hardness of the raceway in comparison with bearings made from bainitic steel or case-hardened steel. Measurements of TL specification steel revealed a hardness of 710-720 HV (60.5-61.0 HRc). This value compares favourably against bearing steel with dimensional stabilised treatment (690-700 HV, 59.5-60.0 HRc), bearing steel with bainite treatment (670-680 HV, 58.5-59.3 HRc) and carburised steel with dimensional stabilised treatment (680-700 HV, 59-60 HRc).

NSK’s proprietary material heat treatment technology also serves to support dimensional stability at high temperatures, as demonstrated by further tests. Bearings made from TL specification steel (at 150°C bearing temperature) showed a negligible rate of dimensional change (around 0.002%) after 10,000 hours – less than bearing steel with dimension stabilising treatment (at 130°C) and far less than bearing steel with standard heat treatment.


Proven advantages

Ultimately, NSK TL specification bearing steel provides 60% more hoop stress resistance and five times the fatigue life of bearing steel with bainite treatment, and 180% more hoop stress and twice the fatigue life of bearing steel with standard heat treatment. These performance advantages translate into higher productivity and genuine competitive gain for users.

The popularity of TL series bearings is rising across Europe. For instance, a well-known Russian company in the paper industry that wanted to modernise its cardboard-making machine has recently taken delivery of TL series spherical roller bearings for 108 drying cylinders (drive and non-drive side). Excellent performance and product characteristics were the predominant reasons behind the purchase decision. Many TL series bearings are also in service within the drying sections of paper and cardboard-making machines at other plants in Russia, including for a felt roll application.

With increasing numbers of machinery manufacturers and paper mills seeking to maximise operating life and uptime, NSK today produces over 100 different TL bearing sizes/types, helping a wide range of customers achieve better and more cost-effective performance. 

 

Picture 1):  NSK spherical roller bearings with TL technology deliver twice the service life of conventional counterparts

Performance gains available with NSK TL series bearings

Picture 2): Inner ring fracture test results indicate the performance gains available with NSK TL series bearings

Longer life available with NSK TL spherical roller bearings

Picture 3): The longer life available with NSK TL spherical roller bearings is clear to see from a series of benchmark tests

Contact Search

Search By
Search by keywords or select from the filter list