Bearings - 05/12/2022
Preventing electrical erosion of bearings in EV drivetrains

NSK currently developing a new and cost-effective way of preventing electrical erosion in the drivetrains of electric vehicles (EVs). Based on a unique method of producing a patented plastic over-moulding for deep groove ball bearings, EV manufacturers will make significant savings in comparison with expensive ‘hybrid’ bearings that feature insulating components made from ceramics.
Parasitic current can take many paths through an EV motor due to circumstances such as the presence of an inverter that switches frequently across multiple phases. Specific types of electric motor architecture can also cause a variety of bearing current flows, including rotor ground bearing currents, circulating bearing currents and EDM (electrical discharge machining) currents.
EDM currents, in particular, present a severe risk to bearings, largely due to arcing that occurs at specific voltages. This arcing (load charging) leads to uncontrolled discharging at fairly high ampere values, essentially changing the morphology of the steel bearing rings and balls. Here, material melts and re-solidifies on the metal surface so that ripples several microns deep begin to appear on the bearing raceways of both the inner and outer ring. Excessive noise is often the first indicator of this issue. For EVs, which are becoming more silent with ongoing development, noise is highly undesirable.
NSK decided it was time to set about developing a solution to this long-standing problem, firstly by assessing the conditions that promote electrical erosion, including: operating conditions such as load, rotational speed, temperature and lubricant viscosity; the condition of the resulting lubrication (hydrodynamic, mixed, boundary); and electrical properties like resistance (material and capacitive).
Established methods to help prevent electrical erosion essentially comprise either insulation or conduction. If the charges are not too high, it might be sufficient to employ a conductive grease, or well-dimensioned grounding elements. However, for specific bearing positions, such as the drive-end bearing prior to the gearbox, insulation is required in the form of either ceramic or plastic bearing components. For instance, NSK can use ceramic as a coating on the outer/inner rings, or can manufacture the entire roller elements and balls from ceramic. Although these ‘hybrid’ bearings provide an optimal countermeasure to electrical erosion, they are also expensive.
The requirement for a more cost-effective solution is pressing because the high-voltage architecture of EVs is about to change from the 400V systems that are dominant today, to 800V. The latter will potentially command 50% of the market as soon as 2030, which will simply double the issue and require even better protection measures for bearings.
NSK is therefore proposing the use of a plastic over-moulding made from a high-performance a PPS (polyphenylene sulphide) polymer that offers high resistance against heat and a large variety of chemicals, as well as stable electrical and mechanical performance (even at temperatures up to 150°C). In addition, the material provides a low level of water absorption, unlike many other polymer types, ensuring dimensional stability.
Comprehensive NSK tests reveal the performance of the over-moulded bearings in comparison with the company’s standard bearings. For example, at 24V voltage and 15kHz frequency, standard bearings showed clear electrical erosion of the inner and outer rings. In contrast, the new NSK over-moulded bearings demonstrated no evidence of this phenomenon. The same outcome resulted at various rotational speeds.
Production of the over-moulding comes courtesy of an innovative injection moulding process located at an NSK facility in Europe to optimise supply to the EV industry. Special mould features ensure homogenous distribution and orientation of the molecules and glass fibres to optimise mechanical performance. Notably, the precision of the over-moulding means there is no requirement for grinding, leaving a ‘structured’ finish in place. As a result there is not 100% contact between the housing and the outside diameter of the bearing, creating gaps filled with air. Air is a good isolator and costs nothing. This innovation provides market differentiation for the NSK solution. As a further benefit, the structured finish overcomes the established issue of bearing creep within housings, as it potentially provides a better fit due to multiple contact points (depending on the use case).
Applicable on the inner and outer ring, the patented insulation layer will usually range from 0.7 to 1.2mm in thickness. To accommodate the extra material NSK can offer space-neutral solutions. This is easiest when starting a new bearing design, although NSK can also machine material from the outer diameter of existing bearings accordingly. However, there is a cost element to this solution. As an alternative proposal, OEMs can look to open up the housing that accommodates the bearing, which means NSK will not have to change its process. Taking this pathway allows EV manufacturers to take full advantage of the significant cost savings available in comparison with hybrid bearings.
At last, the EV industry has a cost-effective solution that negates the electrical erosion of bearings in electrified drivetrains. The over-moulding is currently applicable to NSK’s 6008 and soon for its 6206 deep groove ball bearing series (sealed and non-sealed), which are ideal for EV applications.
As a final note, NSK has a modular test mould available that covers outer diameters from 55-95mm (up to 30mm width). The company is therefore ready to undertake tests on behalf of customers with requirements in this range.
Picture 1): Applicable on the inner and outer ring, the patented insulation layer thickness ranges from 0.7 to 1.2mm.

Picture 2): NSK tests reveal the success of the over-moulded bearing innovation against standard NSK bearings
Contact Search
NSK LTD. HEADQUARTERS
- Phone: +81-3-3779-7111
- Fax: +81-3-3779-7431
- Nissei Bldg. 1-6-3 Ohsaki, Shinagawa-ku, Tokyo 141-8560, Japan
NSK LTD. FUJISAWA PLANT
- Phone: +81-466-21-3111
- Fax: +81-466-25-1209
- 1-5-50 Kugenumashinmei, Fujisawa-shi, Kanagawa 251-8501, Japan
NSK LTD. FUJISAWA PLANT KIRIHARA
- Phone: +81-466-43-3800
- Fax: +81-466-43-3816
- 12 Kirihara-cho, Fujisawa-shi, Kanagawa 252-0811, Japan
NSK LTD. KIRIHARA PRECISION MACHINERY PLANT
- Phone: +81-466-44-3505
- Fax: +81-466-52-7684
- 12 Kirihara-cho, Fujisawa-shi, Kanagawa 252-0811, Japan
NSK LTD. FUKUSHIMA PLANT
- Phone: +81-247-33-3210
- Fax: +81-247-33-3114
- 180-1 Nikaki Tsutsumi Tanagura-machi, Higashishirakawa-gun, Fukushima 963-6101, Japan
NSK LTD. TAKASAKI PLANT
- Phone: +81-27-343-6431
- Fax: +81-27-344-7350
- 358 Yawata-machi, Takasaki-shi, Gunma 370-0884, Japan
NSK LTD. HARUNA PLANT
- Phone: +81-27-360-8511
- Fax: +81-27-360-8557
- 941-2 Nakazatomi-machi, Takasaki-shi, Gunma 370-3344, Japan
NSK LTD. ISHIBE PLANT
- Phone: +81-748-77-3161
- Fax: +81-748-77-5875
- 1-1-1 Ishibegaoka, Konan-shi, Shiga 520-3180, Japan
NSK LTD. OHTSU PLANT
- Phone: +81-77-537-1600
- Fax: +81-77-537-1609
- 1-16-1 Seiran, Ohtsu-shi, Shiga 520-0833, Japan
NSK LTD. SAITAMA PLANT
- Phone: +81-48-565-1111
- Fax: +81-48-565-1420
- 1-1 Ohnuma, Hanyu-shi, Saitama 348-8506, Japan
NSK LTD. SAITAMA PRECISION MACHINERY PLANT
- Phone: +81-48-565-1117
- Fax: +81-48-565-1118
- 1-1 Ohnuma, Hanyu-shi, Saitama 348-8506, Japan
NSK MACHINERY CO., LTD. HEAD OFFICE
- Phone: +81-480-85-3131
- Fax: +81-480-85-6924
- 5 Showanuma Shobu-machi, Kuki-shi, Saitama 346-0198, Japan
NSK MICRO PRECISION CO., LTD. HEAD OFFICE
- Phone: +81-3-5283-7420
- Fax: +81-3-5259-0882
- 6F Hirose Bldg. 3-17 Kanda-Nishikicho, Chiyoda-ku, Tokyo 101-0054, Japan
NSK MICRO PRECISION CO., LTD. Matsukawa Plant
- Phone: +81-265-36-3315
- 2953 Moto-Ojima Matsukawa-machi, Shimoina-gun, Nagano 399-3303, Japan
NSK STEERING SYSTEMS CO., LTD. Soja Plant, Akagi Manufacturing Dept.
- Phone: +81-27-268-1000
- Fax: +81-27-268-1003
- 1240-1 Iidoi-machi, Maebashi-shi, Gunma 379-2111, Japan
NSK STEERING SYSTEMS CO., LTD. Soja Plant, Soja Manufacturing Dept.
- Phone: +81-27-253-1331
- Fax: +81-27-253-0778
- 1-8-1 Soja-machi, Maebashi-shi, Gunma 371-8528, Japan
NSK Steering & Control INC. HEADQUARTERS
- Phone: +81-3-5434-9052
- Fax: +81-3-5434-9057
- Nissei Bldg. 1-6-3 Ohsaki, Shinagawa-ku, Tokyo 141-0032, Japan
NSK-WARNER K.K. FUKUROI PLANT
- Phone: +81-538-43-1121
- Fax: +81-538-43-1595
- 2345 Aino, Fukuroi-shi, Shizuoka 437-8545, Japan
NSK KYUSHU CO., LTD. HEAD OFFICE
- Phone: +81-943-77-3110
- Fax: +81-943-77-7506
- 774 Aza Nissei Furukawa Ukiha-machi, Ukiha-shi, Fukuoka 839-1405, Japan
NSK (CHINA) INVESTMENT CO., LTD.
- Phone: +86-512-5796-3000
- Fax: +86-512-5796-3300
- No.8 NSK Rd. Huaqiao Economic Development Zone, Kunshan, Jiangsu 215332, China
NSK (CHINA) RESEARCH & DEVELOPMENT CO., LTD.
- Phone: +86-512-5796-3000
- Fax: +86-512-5796-3300
- No.8 NSK Rd. Huaqiao Economic Development Zone, Kunshan, Jiangsu 215332, China
NSK (SHANGHAI) TRADING CO., LTD.
- Phone: +86-512-5796-3000
- Fax: +86-512-5796-3300
- No.8 NSK Rd. Huaqiao Economic Development Zone, Kunshan, Jiangsu 215332, China
NSK CHINA SALES CO., LTD.
- Phone: +86-512-5796-3000
- Fax: +86-512-5796-3300
- No.8 NSK Rd. Huaqiao Economic Development Zone, Kunshan, Jiangsu 215332, China
NSK (CHINA) INVESTMENT CO., LTD. BEIJING BRANCH
- Phone: +86-10-6590-8161
- Fax: +86-10-6590-8166
- Room 1906 Beijing Fortune Bldg. No.5 Dong SanHuan BeiLu, Chao Yang District, Beijing, Beijing 100004, China
NSK (CHINA) INVESTMENT CO., LTD. TIANJIN BRANCH
- Phone: +86-22-8319-5030
- Fax: +86-22-8319-5033
- Unit 4604,46/F., Metropolitan Tower, 183 Nanjing Road, Heping District, Tianjin, Tianjin 300050, China
NSK (CHINA) INVESTMENT CO., LTD. SHENYANG BRANCH
- Phone: +86-24-2550-5017
- Fax: +86-24-2334-2058
- No.7, 15 Street Shenyang Economic & Technological Development Area, Shenyang, Liaoning 110141, China
NSK (CHINA) INVESTMENT CO., LTD. CHANGCHUN BRANCH
- Phone: +86-431-8898-8682
- Fax: +86-431-8898-8670
- Room 902-03, Changchun Hongwell International Plaza, No.3299 Renmin Street, Changchun, Jilin 130061, China
NSK (CHINA) INVESTMENT CO., LTD. DALIAN BRANCH
- Phone: +86-411-8800-8168
- Fax: +86-411-8800-8160
- Room1805 Xiwang Tower, No.136 Zhongshan Road, Zhongshan District, Dalian, Liaoning 116001, China
NSK (CHINA) INVESTMENT CO., LTD. NANJING BRANCH
- Phone: +86-25-8472-6671
- Fax: +86-25-8472-6687
- Room A1 22F, Golden Eagle International Plaza, No.89 Hanzhong Road, Nanjing, Jiangsu 210029, China
NSK (CHINA) INVESTMENT CO., LTD. QINGDAO BRANCH
- Phone: +86-532-5568-3877
- Fax: +86-532-5568-3876
- Room 802, Farglory International Plaza, No.26 Xianggang Zhong Road, Shinan District, Qingdao, Shandong 266071, China
NSK (CHINA) INVESTMENT CO., LTD. GUANGZHOU BRANCH
- Phone: +86-20-3817-7800
- Fax: +86-20-3786-4501
- Room 1011-16, Yuexiu Financial Tower, No.28 Zhujiang Road East, Zhujiang New Town, Guangzhou, Guangdong 510627, China
NSK (CHINA) INVESTMENT CO., LTD. CHANGSHA BRANCH
- Phone: +86-731-8571-3100
- Fax: +86-731-8571-3255
- Room 3209, Huayuan International Center, No.36, Section 2, Xiangjiang Middle Road, Tianxin District, Changsha, Hunan 410002, China
NSK (CHINA) INVESTMENT CO., LTD. LUOYANG BRANCH
- Phone: +86-379-6069-6188
- Fax: +86-379-6069-6180
- Room 408, Building A, Zhong hong Excellence Center, No.1 Wu huan Street, Luo long District, Luoyang, Henan 471000, China
NSK (CHINA) INVESTMENT CO., LTD. FUZHOU BRANCH
- Phone: +86-591-8380-1030
- Fax: +86-591-8380-1225
- Room 1801-1811, B1#1A Class Office Building, Wanda Plaza, No.8 Aojiang Road, Fuzhou, Fujian 350009, China
NSK (CHINA) INVESTMENT CO., LTD. WUHAN BRANCH
- Phone: +86-27-8556-9630
- Fax: +86-27-8556-9615
- Room 1512, No.198 Yuncai Road, Office Building, Oceanwide City Square, Jianghan District, WuHan, Hubei 400039, China
NSK (CHINA) INVESTMENT CO., LTD. CHENGDU BRANCH
- Phone: +86-28-8528-3680
- Fax: +86-28-8528-3690
- Room 1117, Lippo Tower, NO.62 North Kehua Road, Chengdu, Sichuan 610041, China
NSK (CHINA) INVESTMENT CO., LTD. CHONGQING BRANCH
- Phone: +86-23-6806-5310
- Fax: +86-23-6806-5292
- Room 612, Commercial Apartment, Athestel Hotel, No.288, Keyuan Rd.4, Jiulongpo District, Chongqing, Chongqing 400039, China
NSK (CHINA) INVESTMENT CO., LTD. XI'AN BRANCH
- Phone: +86-29-8765-1896
- Fax: +86-29-8765-1895
- Room 1007, B Changan Metropolls Center, No.88, Nanguanzheng Steet, Xi'an, Shanxi 710068, China
NSK HONG KONG LTD. HONG KONG
- Phone: +852-2739-9933
- Fax: +852-2739-9323
- Suite 705 7th Floor South Tower World Finance Centre Harbour City T.S.T, Kowloon, Hong Kong, China
NSK HONG KONG LTD. SHENZHEN
- Phone: +86-755-2590-4886
- Fax: +86-755-2590-4883
- Room 624-626 6/F Kerry Center Renminnan Road, Shenzhen, Guangdong 518001, China
KUNSHAN NSK CO., LTD.
- Phone: +86-512-5771-5654
- Fax: +86-512-5771-5689
- NO.1268 Middle Huang Pu Jiang Rd, Kunshan Economic & Technology Development Zone, Kunshan, Jiangsu 215335, China
SUZHOU NSK BEARINGS CO.,LTD.
- Phone: +86-512-6665-5666
- Fax: +86-512-6665-9138
- No.22 Taishan Road, Suzhou New District, Suzhou, Jiangsu 215129, China
NSK STEERING SYSTEMS DONGGUAN CO., LTD.
- Phone: +86-769-2262-0960
- Fax: +86-769-2316-2867
- High-tech Park, Shilong Road, Guanlong Section, Dongguan, Guangdong 523119, China
ZHANGJIAGANG NSK PRECISION MACHINERY CO., LTD.
- Phone: +86 512-5867-6496
- Fax: +86 512-5818-0970
- No.134 Zhenxing Road, Yangshe Town, Zhangjiagang, Jiangsu 215600, China
CHANGSHU NSK NEEDLE BEARING CO., LTD.
- Phone: +86-512-5230-1111
- Fax: +86-512-5230-6011
- No.666 Dongnan Road, Changshu New & Hi-tech Industrial Development Zone, Changshu, Jiangsu 215500, China
NSK HANGZHOU AUTOMOTIVE COMPONENTS CO., LTD.
- Phone: +86-571-8231-4818
- Fax: +86-571-8248-6656
- No.308, Gaoxin 11th Road, Qiaonan Area, Xiaoshan Economic and Technological Development Zone, Xiaoshan District, Hangzhou, Zhejiang 311231, China
SHENYANG NSK PRECISION CO., LTD.
- Phone: +86-24-2550-5017
- Fax: +86-24-2532-6082
- No.7, 15 Street, Shenyang Economic & Technological Development Area, Shenyang, Liaoning 110141, China
SHENYANG NSK CO., LTD.
- Phone: +86-24-2532-6080
- Fax: +86-24-2532-6081
- No.5, 15 Street, Shenyang Economic & Technological Development Area, Shenyang, Liaoning 110141, China
HEFEI NSK CO., LTD.
- Phone: +86-551-6856-2811
- Fax: +86-551-6856-2928
- No.89, Chuangxin Avenue, Boyan Science and Technology Park, High-tech Zone, Hefei, Anhui 230088, China
NSK HANGZHOU AUTOMOTIVE ELECTRONIC TECHNOLOGY CO., LTD.
- Phone: +86-571-8231-4818
- Fax: +86-571-8248-6656
- No.308, Gaoxin 11th Road, Qiaonan Area, Xiaoshan Economic and Technological Development Zone, Xiaoshan District, Hangzhou, Zhejiang 311231, China
NSK DONGGUAN AUTOMOTIVE TECHNOLOGY CO., LTD.
- Phone: +86-769-2226-6639
- 1-101Room, Building 25, No. 77, Shilong Road, Guancheng Street, Dongguan, Guangdong 523119, China
NSK-WARNER (SHANGHAI) CO., LTD.
- Phone: +86-21-3365-5757
- Fax: +86-21-3365-5262
- No. 2518 Huancheng Road (West) Fengxian District, Shanghai, Shanghai 201401, China
AKS PRECISION BALL (HANGZHOU) CO., LTD.
- Phone: +86-571-2280-1288
- Fax: +86-571-2280-1268
- No. 189 Hongda Road Xiaoshan Area of Economic & Technological Development Zone, Hangzhou, Zhejiang 311231, China
NSK AUTOMOTIVE COMPONENTS CO., Ltd.
- Phone: +86-512-5796-3000
- Fax: +86-512-5796-3300
- No.8 NSK Rd., Huaqiao Economic Development Zone, Kunshan, Jiangsu 215332, China
TAIWAN NSK PRECISION CO., LTD. TAIPEI
- Phone: +886-2-2772-3355
- Fax: +886-2-2772-3300
- 10F-A6 No.168Sec.3 Nanjing East Rd. Zhongshan Dist., Taipei City, 104, Taiwan
TAIWAN NSK PRECISION CO., LTD. TAICHUNG
- Phone: +886-4-2708-3393
- Fax: +886-4-2708-3395
- 3F.-2 No.540Sec.3 Taiwan Blvd. Xitun Dist., Taichung City, 407, Taiwan
TAIWAN NSK PRECISION CO., LTD. TAINAN
- Phone: +886-6-215-6058
- Fax: +886-6-215-5518
- Rm. A1 9F.No.189 Sec. 1 Yongfu Rd. West Central Dist., Tainan City, 700, Taiwan
NSK KOREA CO., LTD. CHANGWON PLANT
- Phone: +82-55-287-6001
- Fax: +82-55-285-9982
- 53 Gongdan-ro 474 beon-gil Seongsan-gu, Changwon-si, Gyeongsangnam-do 51575, Korea
NSK KOREA CO., LTD. SEOUL
- Phone: +82-2-3287-0300
- Fax: +82-2-3287-0345
- Posco Center (West Wing) 9F Western-wing Teheran-ro, Gangnam-gu, Seoul 6194, Korea
NSK KOREA CO., LTD. CHEONAN PLANT
- Phone: +82-41-411-6000
- Fax: +82-41-411-6030
- 11 5Sandan 7-Ro Susin-myeon Dongnam-gu, Cheonan-si, Chungcheongnam-do 31251, Korea
NSK BEARINGS INDIA PRIVATE LTD. HEAD OFFICE
- Phone: +91-44-28479600
- TVH Beliciaa Towers 2nd Floor BlockI No.71/1 MRC Nagar Main Road, MRC Nagar, Chennai, Tamil Nadu 600028, India
NSK BEARINGS INDIA PRIVATE LTD. GURGAON BRANCH
- Phone: +91-124–4838000
- Unit No. 202 2nd Floor ‘A’ Block Iris Tech Park Sector–48 Sohna Road, Gurgaon, Haryana 122018, India
NSK BEARINGS INDIA PRIVATE LTD. MUMBAI BRANCH
- Phone: +91-9987617968
- 91 Spring Board Business Hub Private Limited, Godrej & Boyce, Gate No 2, Plant No 6, LBS Marg, Opposite Vikhroli Bus Depot, Vikhroli West, Mumbai, Maharashtra 400079, India
NSK BEARINGS INDIA PRIVATE LTD. JAMSHEDPUR BRANCH
- Phone: +91-657–2421144
- 36 Maharani Mansion Ground Floor Circuit House Area P.O. Bistupur East Singhbhum, Jamshedpur, Jharkhand 831001, India
NSK BEARINGS INDIA PRIVATE LTD. CHENNAI PLANT
- Phone: +91-44-27143000
- Plot No.A2 SIPCOT Growth Centre Oragadam Mathur Village Sriperumbudur Taluk Kancheepuram District, Tamil Nadu, 602105, India
NSK INTERNATIONAL (SINGAPORE) PTE LTD. SINGAPORE
- Phone: +65-6496-8000
- Fax: +65-6250-0247
- 238A Thomson Road #24-01/02, Novena Square Tower A, 307684, Singapore
NSK BEARINGS (THAILAND) CO., LTD. BANGKOK
- Phone: +66-2320-2555
- Fax: +66-2320-2826
- 26 Soi Onnuch 55/1 Pravet Subdistrict Pravet District, Bangkok, 10250, Thailand
SIAM NSK STEERING SYSTEMS CO., LTD. OFFICE/PLANT
- Phone: +66-38-522-343
- Fax: +66-38-522-351
- 90 Moo 9 Wellgrow Industrial Estate Km. 36 Bangna-Trad Rd. Bangwao, Bangpakong, Chachoengsao 24130, Thailand
NSK BEARINGS MANUFACTURING (THAILAND) CO., LTD. OFFICE/PLANT
- Phone: +66-38-454-010
- Fax: +66-38-454-017
- 700/430 Moo 7 Amata City Chonburi Industrial Estate T.Donhualor A.Muang, Chonburi, Chonburi 20000, Thailand
NSK ASIA PACIFIC TECHNOLOGY CENTRE (THAILAND) CO., LTD. CHONBURI
- Phone: +66-38-454-631
- Fax: +66-38-454-634
- 700/430 Moo 7 Amata City Chonburi Industrial Estate T.Donhualor A. Muangchonburi, Chonburi, Chonburi 20000, Thailand
PT. NSK INDONESIA JAKARTA
- Phone: +62-21-252-3458
- Fax: +62-21-252-3223
- Summitmas II 4th Floor JI. Jend Sudirman Kav. 61-62, Jakarta, 12190, Indonesia
PT. NSK BEARINGS MANUFACTURING INDONESIA JAKARTA PLANT
- Phone: +62-21-898-0155
- Fax: +62-21-898-0156
- Kawasan MM. 2100 Blok M-4 Desa Gandamekar Kecamatan Cikarang Barat Kabupaten, Bekasi, 17520, Indonesia
PT.NSK-WARNER INDONESIA BEKASI
- Phone: +62-21-8998-3216
- Fax: +62-21-8998-3218
- Block DD-12 MM2100 Industrial Town Cikarang Barat, Bekasi, 17520, Indonesia
PT.AKS PRECISION BALL INDONESIA BEKASI
- Phone: +62-21-8998-2248
- Fax: +62-21-8998-2101
- Blok N-8 Kwasan Berikat MM2100 Industrial Town Cikarang Barat, Bekasi, 12190, Indonesia
NSK BEARINGS (MALAYSIA) SDN.BHD. HEAD OFFICE
- Phone: +60-3-5886-3388
- No. 12A Jalan Subang 7/4 Taman Perindustrian Subang USJ1 Subang, Jaya, Selangor Darul Ehsan 47600, Malaysia
NSK BEARINGS (MALAYSIA) SDN.BHD. PRAI
- Phone: +60-3-5886-3388
- No. 24 Jalan Kikik Taman Inderawasih, Prai, Penang 13600, Malaysia
NSK BEARINGS (MALAYSIA) SDN.BHD. JOHOR BAHRU
- Phone: +60-3-5886-3388
- 88 Jalan Ros Merah 2/17 Taman Johor Jaya, Johor Bahru, Johor 81100, Malaysia
NSK MICRO PRECISION (M) SDN.BHD. MALAYSIA PLANT
- Phone: +60-3-8961-6288
- Fax: +60-3-8961-6488
- No.43 Jalan Taming Dua Taman Taming Jaya BalakongSelangor, Darul, Ehsan 43300, Malaysia
ISC MICRO PRECISION SDN.BHD. KUALA LUMPUR
- Phone: +60-12-338-5221
- No. 108 Jalan Taming LimaTamanTamingJaya, Balakong, Selangor Darul Ehsan 43300, Malaysia
ISC MICRO PRECISION SDN.BHD. IPOH
- Phone: +60-5-323-1020
- Fax: +60-5-323-1021
- Lot 1 3&5PersiaranPerindustrianPengkalan17 Pengkalan Maju Industrial Park, Ipoh, Perak Darul Ridzuan 31500, Malaysia
NSK VIETNAM CO., LTD. HEAD OFFICE
- Phone: +84-24-3955-0159
- Fax: +84-24-3955-0158
- Techno Center Room 204-205 Thang Long Industrial Park Dong Anh District, HanoiVietnam
NSK VIETNAM CO., LTD. HO CHI MINH CITY REPRESENTATIVE OFFICE
- Phone: +84-28-3822-7907
- Fax: +84-28-3822-7910
- Unit 609 The Landmark Building 5B TonDuc Thang Street District 1, Ho Chi Minh CityVietnam
NSK INTERNATIONAL (SINGAPORE) PTE LTD. PHILIPPINES REPRESENTATIVE OFFICE (MANILA)
- Phone: +63-2-893-9543
- Fax: +63-2-893-9173
- 8th Floor The Salcedo Towers 169 H.V. Dela Costa St. Salcedo Villege, Makati City, 1227, Philippines
NSK AUSTRALIA PTY. LTD. MELBOURNE
- Phone: +61-3-9765-4400
- Fax: +61-3-9765-4466
- 100 Logis Boulevard, Dandenong South, Victoria 3175, Australia
NSK AMERICAS, INC. HEADQUARTERS
- Phone: 888-446-5685
- Fax: +1-734-913-7511
- 4200 Goss Road, Ann Arbor, Michigan 48105, U.S.A.
NSK AMERICAS TECHNOLOGY CENTER
- Phone: 888-446-5675
- Fax: +1-734-913-7511
- 4200 Goss Road, Ann Arbor, Michigan 48105, U.S.A.
NSK CORPORATION CLARINDA PLANT
- Phone: +1-712-695-2721
- 1100 N. First Street, Clarinda, Iowa 51632, U.S.A.
NSK CORPORATION FRANKLIN PLANT
- Phone: +1-317-738-5000
- Fax: +1-317-738-5064
- 3400 Bearing Drive, Franklin, Indiana 46131, U.S.A.
NSK CORPORATION LIBERTY PLANT
- Phone: +1-765-458-5000
- Fax: +1-765-458-7832
- 1112 East Kitchel Road, Liberty, Indiana 47353, U.S.A.
NSK PRECISION AMERICA, INC.
- Phone: +1-317-738-5000
- Fax: +1-317-738-5050
- 3450 Bearing Drive, Franklin, Indiana 46131, U.S.A.
NSK PRECISION AMERICA, INC. SAN JOSE
- Phone: +1-408-944-9400
- Fax: +1-408-944-9405
- 780 Montague Expressway, San Jose, California 95131, U.S.A.
NSK LATIN AMERICA, INC. MIRAMAR
- Phone: +1-305-477-0605
- Fax: +1-305-477-0377
- 3350 SW 148th Ave Suite 420, Miramar, 33027, U.S.A.
NSK STEERING SYSTEMS AMERICA, INC. OFFICE/PLANT
- Phone: +1-802-442-5448
- Fax: +1-802-442-2253
- 110 Shields Drive, Bennington, Vermont 05201, U.S.A.
NSK STEERING SYSTEMS AMERICA, INC. ANN ARBOR
- Phone: 42.2947579941068
- Fax: +1-734-913-7102
- 4200 Goss Road, Ann Arbor, Michigan 48105, U.S.A.
NSK STEERING SYSTEMS AMERICA, INC. DYERSBURG PLANT
- Phone: +1-731-288-3000
- Fax: +1-731-288-3001
- 2962 Fort Hudson Road, Dyersburg, Tennessee 38024, U.S.A.
BK Vibro America Inc.
- Phone: +1-775-552-3110
- 1100 Mark Circle, Gardnerville, Nevada 89410, U.S.A.
NSK-AKS PRECISION BALL COMPANY CLARINDA
- Phone: +1-712-695-2915
- 1100A North First Street, Clarinda, Iowa 51632, U.S.A.
NSK CANADA INC.
- Phone: +1-888-603-7667
- Fax: +1 905-890-1938
- 317 Rutherford Road South, Brampton, Ontario L6W 3R5, Canada
NSK RODAMIENTOS MEXICANA, S.A. DE C.V.
- Phone: +52-472-500-9500
- Fax: +52-472-103-9403
- Email: infomex@nsk.com
- Circuito Mexiamora Oriente No. 331 Parque Industrial Santa Fe I Puerto Interior, Silao, Guanajuato 36275, Mexico
NSK BEARINGS MANUFACTURING MEXICO S.A. DE C.V.
- Phone: +52-472 103 9400
- Fax: +52-472 103 9401
- Email: infomex@nsk.com
- Circuito Mexiamora Oriente No.331 Parque Industrial Santa Fe I Col. Puerto Interior, Silao, Guanajuato 36275, Mexico
NSK-Warner MEXICO, S.A. de C.V.
- Phone: +52-472-478-3600
- Avenida Purina No 35 Fraccionamiento Mineral de Pozos Col. Puerto Interior, Silao, Guanajuato 36275, Mexico
AKS PRECSION BALL MEXICO S.A. DE C.V.
- Phone: +52-472-103-9466
- Circuito Mexiamora Oriente 331 Parque Industrial Santa Fe V. Col. Puerto Interior, Silao, Guanajuato, Mexico
NSK BRASIL LTDA. HEAD OFFICE AND PLANT
- Phone: +55-11-4744-2500
- Av. Vereador João Batista Fitipaldi, nº 66 - Vila Maluf, Suzano, São Paulo 08685-000, Brazil
NSK ARGENTINA SRL BUENOS AIRES
- Phone: +54 11 4704-5100
- García del Río 2477 - Piso 7º - Oficina "A" - C1429DEA - C.A.B.A, Buenos Aires, 1429, Argentina
NSK PERU S.A.C. LIMA
- Phone: +51-1-493-4385
- Email: nskenespanol@nsk.com
- Calle Teniente Enrique Palacious Nro.360 Oficina 311 Miraflores, LimaPeru
NSK UK Ltd.
- Phone: +44 1636605123
- Email: info-uk@nsk.com
- Northern Road, Nottinghamshire, NG24 2JF, United Kingdom
NSK BEARINGS EUROPE LTD. PETERLEE PLANT
- Phone: +44-191-586-6111
- Fax: +44-191-586-3482
- 3 Brindley Road South West Industrial Estate, Peterlee, Co. Durham SR8 2JD, U.K.
AKS PRECISION BALL EUROPE LTD
- Phone: +44-191-587-0000
- Fax: +44-191-587-2027
- Davy Drive NW Industrial Estate, Peterlee, Co. Durham SR8 2PP, U.K.
NSK Deutschland GmbH
- Phone: +49 21024810
- Fax: +49 21024812290
- Email: info-de@nsk.com
- Harkortstrasse 15, Ratingen, 40880, Germany
Brüel & Kjær Vibro GmbH
- Phone: +49-6151-4280
- Leydheckerstrasse 10, Darmstadt, 64293, Germany
NSK France S.A.S.
- Phone: +33(0)130573939
- Fax: +33(0)130570001
- Email: info-fr@nsk.com
- 2, Rue Georges Guynemer, Guyancourt, 78280, France
NSK Spain S.A.
- Phone: +34 932892763
- Fax: +34 934335776
- Email: info-es@nsk.com
- Av. de la Vía Augusta 85 3ª planta / Sant Cugat del Vallés, Barcelona, 08174, Spain
NSK Italia S.p.A.
- Phone: +39 02995191
- Fax: +39 0299025778
- Email: info-it@nsk.com
- Via Garibaldi 215, Garbagnate Milanese (MI), 20024, Italy
NSK European Distribution Centre B.V.
- Phone: +31 (0) 13 4641 050
- Fax: +31 (0) 13 4641 082
- Email: info-nl@nsk.com
- Brakman 54, Tilburg, 5047 SW, The Netherlands
NSK Polska Sp. z o.o.
- Phone: +48 226451525
- Fax: +48 226451529
- Email: info-pl@nsk.com
- MIGDAŁOWA 4/73, Warszawa, 02-796, Poland
NSK NEEDLE BEARING POLAND SP.Z O.O. OFFICE/PLANT
- Phone: +48-41-345-2469
- Fax: +48-41-345-0361
- UL. Jagiellonska 109, Kielce 25-734, Poland
NSK BEARINGS POLSKA S.A. PLANT
- Phone: +48-41-3670502
- Fax: +48-41-367-0500
- Ul. Jagiellonska 109, Kielce 25-734, Poland
AKS PRECISION BALL POLSKA SP. ZO.O
- Phone: +48-74-649-9200
- Fax: +48-74-649-9201
- Ul. Przemyslowa 12, Zarow 58-130, Poland
NSK Rulmanları Orta Doğu Tic.Ltd. Şti
- Phone: +90 2165000675
- Fax: +90 2165000676
- Email: turkey@nsk.com
- Cevizli Mahallesi D-100 Güney Yanyolu Kuriş Kule İş Merkezi, No:2 Kat:4, 34846 Kartal, Türkiye, Istanbul, 34846, Turkey
NSK Bearings Gulf Trading Co.
- Phone: +971 48048200
- Fax: +971 48847227
- Email: info-me@nsk.com
- Dubai, JAFZA View 19, Floor 24 Office LB192402/3 PO Box 262163, Downtown Jebel Ali, United Arab Emirates
Brüel & Kjær Vibro A/S
- Phone: +45-6989-0300
- Lyngby Hovedgade 94 5 sal, Lyngby, 2800, Denmark
NSK Europe Limited Maidenhead - Sucursala Ploiesti
- Phone: +40 344 803 210
- Fax: +40 344 803 218
- Email: info-ro@nsk.com
- Bdul Republicii , 178, Ploiesti, Ploiesti – 100072, Romania
NSK South Africa (PTY) Ltd.
- Phone: +27 0114583600
- Fax: +27 114583608
- Email: info-sa@nsk.com
- 25, Galaxy Avenu, Sandton, 2054, South Africa
Share