Bearings - 16/10/2023
NSK bearings adopted in world-class design and calculation software

NSK will begin providing rolling bearing data to MESYS and KISSsoft, two industry-leading companies that develop technical calculation software for engineers engaged in machinery design. The integration of NSK bearing data will accelerate the design process through quick and easy bearing analysis, reducing the time taken to select bearings.
In response to requests from design engineers, NSK rolling bearings will become an integral part of KISSsoft® and MESYS technical calculation software programs, both of which are in use worldwide. With data available from 2023, the ability to select NSK rolling bearings in these software suites will enhance customer convenience and satisfaction.
KISSsoft AG, part of the multi-national Gleason Corporation, develops modular calculation programs for the design, optimisation and verification of machine elements such as gears and transmissions in line with international standards. Similarly, MESYS AG develops software for technical calculations in a variety of mechanical engineering projects, with particular focus on the sizing of machine elements that include ball screws, shafts and more.
The data that NSK provides will initially span five bearing types: deep groove ball bearings, angular contact ball bearings, cylindrical roller bearings, tapered roller bearings and spherical roller bearings. Software users will simply call up NSK bearing information from the database and perform technical calculations involving gears, housings or shafts, for example. Users will also be able to determine factors such as the surface pressure and service life of bearings.
Importantly, NSK can update the data it provides at any time to ensure the delivery of optimal machine design calculations. Moving forward, NSK will supply information for further rolling bearing types.
Picture: Example of a wind turbine gearbox design for analysis with KISSsoft® or MESYS software
Share