Mood, Press, News

Automotive - 02/10/2023

NSK’s anti-electrical-erosion technologies contribute to longer EV range on a single charge.

Following the completion of performance evaluations, NSK can now offer a broader range of anti-electrical-erosion technologies for eAxle bearings used on electric vehicles (EVs). Among the new options are over-moulded bearings and conductive brushes, elevating NSK's ability to meet diverse demands from automotive OEMs as they look to combat electrical erosion and, in turn, improve reliability and extend EV range.

With growing awareness of the world’s urgent climate-change agenda, society and industry are accelerating their journey towards carbon neutrality. The rising demand for EVs means there is a real opportunity to enhance the sustainability of the transport sector, but the success of this endeavour depends heavily on the underlying technologies. For instance, a key issue in ensuring the long operational life of EVs is preventing the electrical erosion of critical eAxle components such as bearings.

Preventing electrical erosion is becoming increasingly difficult due to the higher output of electric motors and higher drive voltages. Here, technologies like insulating ceramic-ball bearings (hybrid bearings) are most effective way of providing electrical insulation, but are not always the optimal solution for high-volume applications such as EVs.

A good alternative is the adoption of plastic over-moulded bearings, which deliver the electrical insulation required for eAxles but at a lower cost than ceramic-ball bearings. Notably, NSK configures its over-moulded bearings to suit the application and any specific requirements. The materials and manufacturing processes would be quite different for an eAxle and those of a railway application, for example.

Another option to resist electrical erosion is the use of conductive brushes. However, trends in eAxle motors are moving towards the use of highly efficient oil-cooled systems, for which conventional conductive brushes are not suitable, especially in combination with high speeds. NSK's new brushes differ in that they offer sufficient conductivity for a wide range of eAxle applications, even those involving cooling oil lubricated environments. As a further benefit, it is possible to incorporate the conductive brush directly into the shaft to save space.

NSK has already completed basic durability evaluations and can now provide customers with proposals for its latest anti-electrical-erosion technologies, including evaluation data, for practical applications.

In summary, the company’s anti-electrical-erosion options cover both insulating and conductive methods to meet a diverse range of design requirements that balance application and volume criteria. These technologies improve reliability and include measures that support the reduction of overall eAxle unit size. They also contribute to lower electricity consumption and longer vehicle range on a single charge.

 

Picture 1): NSK’s anti-electrical-erosion technologies contribute to longer EV range on a single charge. Photo: Herr Loeffler/Shutterstock

NSK plastic over-moulded bearing

Picture 2): Example of an NSK plastic over-moulded bearing. Photo: NSK

Contact Search

Search By
Search by keywords or select from the filter list