News
Results:
All five NSK European production plants sourcing green electricity
(2021-12-20)
All five NSK European production plants sourcing green electricity - NSK has signed a contract with the electricity provider of its two UK manufacturing facilities in Newark (industrial bearings and linear guides) and Peterlee (automotive bearings) that ensures the supply of ‘green electricity’ ...
NSK innovation overcomes long-standing bearing challenge in the mining industry
(2021-12-13)
NSK innovation overcomes long-standing bearing challenge in the mining industry - NSK has used its extensive problem-solving capabilities and experience to provide mines and quarries with the solution to a long-standing problem.
Wave power – using NSK ball screws
(2021-12-06)
Wave power – using NSK ball screws: Swedish start-up company Ocean Harvesting is harnessing a new inexhaustible source of energy.
NSK Life-Lube bearings drive cost-saving improvements in food plants
(2021-11-22)
NSK Life-Lube bearings drive cost-saving improvements in food plants - NSK’s Life-Lube bearing units are proving increasingly popular in the food and beverage industry, and with good reason.
NSK Super-TF spherical roller bearings offer long service life in contaminated environments
(2021-11-15)
NSK Super-TF spherical roller bearings offer long service life in contaminated environments - Unforeseen bearing failures in production-critical machines and equipment can prove extremely costly in replacement parts, labour and downtime, all of which have a negative impact on bottom-line ...
NSK Self-Lube® bearings prove reliable in harsh conditions
(2021-11-05)
NSK Self-Lube® bearings prove reliable in harsh conditions - NSK Self-Lube® bearing units with triple lip seal and end cap protectors provide an extended service life in harsh operating conditions, such as those prevalent within the quarrying, mining and construction sectors.
Achieve competitive gain with NSK TL spherical roller bearings
(2021-10-25)
Achieve competitive gain with NSK TL spherical roller bearings - NSK TL series spherical roller bearings are active across the world in a host of papermaking machinery applications.
NSK ProKIT catalogue now available as PDF download
(2021-10-14)
NSK ProKIT catalogue now available as PDF download - Any companies serving the automotive aftermarket (AAM) can now benefit from the newly released PDF edition of NSK’s ProKIT catalogue.
Changing to NSK Molded-Oil bearings reduces maintenance costs at a car wash
(2021-10-11)
Changing to NSK Molded-Oil bearings reduces maintenance costs at a car wash - The operator of a car wash line in Germany repeatedly had to replace bearings in the rotary unions of the system’s wash heads, leading to costs of over €12,000 per annum for spare parts alone.
Linear Motion Control expands range of miniature linear components for medical equipment
(2021-10-04)
Expansion of miniature linear components for medical equipment - Human beings provide the measure: the drives of surgical robots, blood pumps, and MRI and CT equipment (for example), must offer a design that ensures they perform their tasks very precisely and smoothly without emitting any ...
NSK SWR spherical roller bearings overcome challenges of continuous casting
(2021-09-27)
NSK SWR spherical roller bearings overcome challenges of continuous casting - The bearings used in continuous casting machines have to endure arduous operating conditions that include high temperatures, heavy loads, ultra-low speeds, water/water vapour and scale.
NSK triple lip seal provides ultimate bearing protection
(2021-09-20)
NSK triple lip seal provides ultimate bearing protection - Bearings that operate in conditions with a high degree of contamination must offer many attributes. A highly efficient sealing arrangement is priority number one.
Big performance from small NSK ball screws
(2021-09-13)
Big performance from small NSK ball screws - A new high-speed series of miniature large-lead ball screws from NSK Linear Motion Control offers a number of important benefits to users, including reduced product takt time, the potential to downsize equipment, and reduced power consumption.
Heavy industries gain from NSK spherical roller bearings
(2021-09-06)
Heavy industries gain from NSK spherical roller bearings - NSK produces billions of bearings a year for a myriad of different applications and industries.
Press brake specialist opts for NSK high-load ball screws
(2021-08-30)
Press brake specialist opts for NSK high-load ball screws: Following success with previous-generation machines, a leading manufacturer of press brakes is once again specifying high-quality NSK ball screws for its latest electric model.
NSK Self-Lube® bearing units save steel plant €292,136
(2021-08-23)
NSK Self-Lube® bearing units save steel plant €292,136 - Certain sectors and applications place particularly challenging demands on bearings. Steelmaking is one such example, where the aggressive operating environment means potential bearing failures present a genuine threat to production.
Machining centers feature ball screws with nut cooling to increase surface quality of milled parts
(2021-08-16)
Machining centers feature ball screws with nut cooling to increase surface quality of milled parts - NSK ball screws with nut cooling are setting new standards in the precision of machine tools with mechanical drive components.
Steel plant saves around €70,000 with spherical roller bearings from NSK
(2021-07-19)
Steel plant saves around €70,000 with spherical roller bearings from NSK - For the past four years a hot rolling mill at a steel plant in Spain had been experiencing unexpectedly short bearing life, leading to costly production stoppages.
Machine tool builder benefits from NSK motion control solutions
(2021-07-12)
Machine tool builder benefits from NSK motion control solutions - Euromac, a global specialist in the design and manufacture of punching and bending machines, is benefitting from NSK ball screws, linear guides and bearings in two high-profile recent projects.
Monocarrier units in radiotherapy machines
(2021-07-05)
Monocarrier units in radiotherapy machines - A leading manufacturer of radiotherapy machines is using a Monocarrier linear drive unit from NSK to perform the precise movements and adjustments of the emitter, which projects the finely dosed X-rays or proton beams that kill cancer cells.
Share