News
Results:
Wave power – using NSK ball screws
(2021-12-06)
Wave power – using NSK ball screws: Swedish start-up company Ocean Harvesting is harnessing a new inexhaustible source of energy.
Linear Motion Control expands range of miniature linear components for medical equipment
(2021-10-04)
Expansion of miniature linear components for medical equipment - Human beings provide the measure: the drives of surgical robots, blood pumps, and MRI and CT equipment (for example), must offer a design that ensures they perform their tasks very precisely and smoothly without emitting any ...
Big performance from small NSK ball screws
(2021-09-13)
Big performance from small NSK ball screws - A new high-speed series of miniature large-lead ball screws from NSK Linear Motion Control offers a number of important benefits to users, including reduced product takt time, the potential to downsize equipment, and reduced power consumption.
Press brake specialist opts for NSK high-load ball screws
(2021-08-30)
Press brake specialist opts for NSK high-load ball screws: Following success with previous-generation machines, a leading manufacturer of press brakes is once again specifying high-quality NSK ball screws for its latest electric model.
Machining centers feature ball screws with nut cooling to increase surface quality of milled parts
(2021-08-16)
Machining centers feature ball screws with nut cooling to increase surface quality of milled parts - NSK ball screws with nut cooling are setting new standards in the precision of machine tools with mechanical drive components.
Machine tool builder benefits from NSK motion control solutions
(2021-07-12)
Machine tool builder benefits from NSK motion control solutions - Euromac, a global specialist in the design and manufacture of punching and bending machines, is benefitting from NSK ball screws, linear guides and bearings in two high-profile recent projects.
Monocarrier units in radiotherapy machines
(2021-07-05)
Monocarrier units in radiotherapy machines - A leading manufacturer of radiotherapy machines is using a Monocarrier linear drive unit from NSK to perform the precise movements and adjustments of the emitter, which projects the finely dosed X-rays or proton beams that kill cancer cells.
Automotive plant saves €577,000 a year by switching to NSK linear guides
(2021-06-28)
Automotive plant saves €577,000 a year by switching to NSK linear guides - After suffering an average of four linear guide failures a month on its process-critical component washing machines, a major automotive plant in Mexico is enjoying significant savings having switched to NH series linear ...
Longer operating life with NSK DH/DS series linear guides
(2021-06-07)
Longer operating life with NSK DH/DS series linear guides - With its new long-life DH/DS series, NSK can offer linear guides that achieve twice the running distance of the company’s conventional alternative.
NSK reduces machine tool quadrant glitches during circular interpolation
(2021-05-21)
NSK reduces machine tool quadrant glitches during circular interpolation - The occurrence of machine tool quadrant glitches during circular interpolation routines are an established issue. Thanks to innovation from NSK, it is possible to mitigate the effects of this unwanted phenomenon.
NSK Monocarrier units provide precise and fast handling of medical laboratory samples
(2021-05-06)
NSK Monocarrier units provide precise and fast handling of medical laboratory samples - A manufacturer of automated analytical equipment for medical technology is using a two-axis linear system to handle samples both quickly and precisely.
NSK builds on 30-year MCM partnership with new project success
(2021-04-26)
NSK builds on 30-year MCM partnership with new project success - Successful engineering partnerships are dependent upon many factors, not least trust, innovation, class-leading quality, technical excellence and comprehensive support.
New machine builds on successful IMSA-NSK partnership
(2021-04-12)
New machine builds on successful IMSA-NSK partnership - The new MF1000-3T deep-hole drilling machine from IMSA is taking advantage of the benefits provided by NSK’s DIN-standard ball screws for the European machine tool market.
NSK linear guides help ETEL bring speed and precision to semiconductor manufacturing
(2021-03-29)
NSK linear guides help ETEL bring speed and precision to semiconductor manufacturing - NH series linear guides from NSK are helping a manufacturer of motion platforms for semiconductor manufacturing to provide its customers with a solution that offers speed and precision beyond previous ...
Tschudin Cube 350 centreless grinder uses NSK RA high-precision roller guides
(2021-03-15)
Tschudin Cube 350 centreless grinder uses NSK RA high-precision roller guides - The new Tschudin Cube 350 centreless grinding machine is using NSK’s RA series of low-friction, high-rigidity roller guides, where they are helping to generate excellent levels of surface finish on machined workpieces.
Sourcing linear motion solutions from NSK’s global manufacturing sites: the benefits of an international production network
(2021-02-25)
Sourcing linear motion solutions from NSK’s global manufacturing sites: the benefits of an international production network - High-precision linear guides are an important product group for NSK's Linear Motion Technology (Seiki) management unit.
NSK roller guides simplify welding of wind turbine towers
(2021-02-22)
NSK roller guides simplify welding of wind turbine towers - A collaboration between NSK and Spain-based Talleres Ganomagoga has led to a major advance in the welding of wind turbine towers.
NSK shows its competency in ultra-fine positioning
(2021-02-08)
NSK shows its competency in ultra-fine positioning - As an expert in motion control, NSK frequently supplies customers with manipulators and positioners that meet micrometre and even nanometre accuracy requirements.
New drive for Megatorque Motor boosts safety and usability
(2021-02-01)
New drive for Megatorque Motor boosts safety and usability - NSK has released an upgraded drive for its PS/PN series of Megatorque Motors that offers even higher levels of safety and usability.
MCA demo cell features NSK Monocarrier linear actuator
(2021-01-25)
MCA demo cell features NSK Monocarrier linear actuator - An NSK distribution partner, MCA linear motion robotics, has built a state-of-the-art linear motion demonstration cell that features NSK Monocarrier technology at its core.
Share