News
Results:
NSK releases new low-particle-emission bearing for servomotors
(2024-08-27)
NSK is introducing a high-performance bearing for servomotors that reduces the emission of particles such as grease and oil. This breakthrough development will contribute to the stable operation of vital industry machines such as robots.
Discover how NSK motion control solutions deliver better machining results
(2024-07-08)
NSK Europe will use the forthcoming AMB 2024 international exhibition to shine the spotlight on its latest solutions for machine tools.
NSK helps European rail industry hit top speed at InnoTrans 2024
(2024-07-02)
NSK will use the forthcoming InnoTrans 2024 international trade fair for transport technology (Berlin, 24-27 September) to showcase how its innovation in bearings can help the European rail industry keep pace with growing consumer demands. s
NSK develops grease degradation diagnosis technology for on-site use
(2024-03-11)
NSK is developing a world-first: a high-accuracy way of rapidly and accurately diagnosing the remaining life of lubricant grease. The company will provide the solution as a mobile app, enabling users to perform the on-site analysis of lubricant condition in bearings and linear motion systems.
NSK develops Active Caster for service robot applications
(2024-01-15)
As part of a drive to get robots into more and more workplaces, operating side-by-side with humans, a team of expert development engineers at global motion control specialist NSK have come up with a novel way to improve the mobility of collaborative robots (cobots): the NSK Active Caster.
World first: ultrasonic testing provides highly accurate bearing life predictions
(2024-01-08)
After years of research and development, NSK is revising the basic dynamic load rating of many bearings by up to double the equivalent rolling contact fatigue life (with no change in design or materials).
NSK bearings help pet food plant raise OEE
(2023-12-04)
When a major UK pet food producer wanted better machine utilisation with the aim of raising its OEE (overall equipment effectiveness) by 3 points, it decided to ask experts at bearing specialist NSK if they could evaluate processes and systems to help with this improvement goal.
Steel mill reaps rewards from adopting NSK bearings
(2023-11-13)
When a steel mill was experiencing regular failures of the bearings on its pilger mill, the plant turned to the expertise and experience of NSK for a robust and economic solution.
NSK bearings adopted in world-class design and calculation software
(2023-10-16)
NSK bearings adopted in world-class design and calculation software - NSK will begin providing rolling bearing data to MESYS and KISSsoft, two industry-leading companies that develop technical calculation software for engineers engaged in machinery design.
NSK bearings deliver major savings at snack food plant
(2023-10-02)
NSK bearings deliver major savings at snack food plant - When a major snack food producer began experiencing repeat failures of the bearings on its cutter lines, a switch to NSK Life-Lube® housed bearing units delivered savings in excess of €130,000, primarily thanks to the elimination of lost ...
Insulation plant saves €648,880 a year with NSK bearings
(2023-09-18)
Insulation plant saves €648,880 a year with NSK bearings - A market-leading manufacturer of insulation products for the construction industry turned to NSK for help in solving repeat bearings failures on its band saws.
NSK bearings lead to significant savings at ore plant
(2023-06-05)
NSK bearings lead to significant savings at ore plant - When NSK solved an overheating issue involving the bearings on a dust extraction fan at an ore preparation plant, it led to annual cost savings of €88,955.
NSK bearings deliver macro benefits in micro applications
(2023-05-29)
NSK bearings deliver macro benefits in micro applications - With the micro-mobility market set to soar in the years through to 2030, NSK is in prime position to help OEMs take advantage of this significant demand.
NSK offers customised pre-assembled bearing units
(2023-05-02)
NSK offers customised pre-assembled bearing units : As part of a new product offer, global bearing specialist NSK is able to produce customised pre-assembled cartridge units for applications requiring extremely precise rotational performance.
NSK bearings save steel wire plant over €1.2m a year
(2023-04-17)
NSK bearings save steel wire plant over €1.2m a year - NSK’s assistance proved vital to a company experiencing repeat failures of bearings fitted to the roller assemblies of its steel wire drawing machinery.
NSK spindle bearings boost reliability at automotive plant
(2023-03-20)
NSK spindle bearings boost reliability at automotive plant: A large manufacturer of automotive engines has significantly improved the reliability of its CNC machining centres by adopting NSK sealed spindle bearings that prevent the ingress of cutting fluid.
NSK bearings prevent failures at global can manufacturer
(2023-03-06)
NSK bearings prevent failures at global can manufacturer: When the world’s largest beverage can manufacturer was experiencing regular, unexpected production stoppages due to the premature failure of spray-head bearings in its coating machines, the company turned to the expertise of NSK.
Pre-assembled NSK bearings save time and money at vibrating screen manufacturer
(2023-02-13)
Pre-assembled NSK bearings save time and money at vibrating screen manufacturer: By switching to NSK pre-assembled, fully integrated bearings, a vibrating screen manufacturer is witnessing annual cost savings of €117,000.
NSK bearings reduce concrete floor manufacturing machine failures to zero
(2023-01-30)
NSK bearings reduce concrete floor manufacturing machine failures to zero: Regular bearing failures in a concrete floor manufacturing machine were leading to extensive downtime, costly lost production, and high maintenance costs.
High-speed, easy-to-handle, long-life ball bearings from NSK
(2023-01-16)
High-speed, easy-to-handle, long-life ball bearings from NSK - The innovative QJ series features a high-strength outer-ring-guided brass cage to facilitate extremely high speeds and improved running accuracy.
Share