News
Results:
Electric injection moulding machines benefit from new NSK ball screws
(2024-02-12)
NSK is introducing its advanced HTF-SRM series, a high-speed, heat-resistant version of its ball screws for high-load drive applications.
Ultra-smooth motion technology for NSK linear guides
(2023-09-04)
Ultra-smooth motion technology for NSK linear guides - NSK’s new ultra-smooth motion technology, developed for the company’s popular general-purpose NH/NS series linear guides, is the world’s first design of its type.
NSK develops world’s first bioplastic retaining piece for ball screws
(2023-06-19)
NSK develops world’s first bioplastic retaining piece for ball screws - Made from 100% renewable biological resources (mainly plants), the use of bioplastic for the new retaining piece reduces carbon footprint by 90% over its lifecycle in comparison with using conventional materials.
NSK transportation ball screws in high demand
(2023-04-03)
NSK transportation ball screws in high demand - Transportation ball screws are popular across industry as a cost-effective alternative to precision ground ball screws.
Tyre manufacturer saves almost €100,000 a year with NSK ball screws
(2023-02-27)
Tyre manufacturer saves almost €100,000 a year with NSK ball screws: When a tyre manufacturer was enduring frequent failures of the ball screw within the air drum of its tyre building machine, the company turned to the expertise of NSK and its HTF series ball screw.
New NSK ball screw for next-generation, high-accuracy machine tools
(2022-11-21)
NSK ball screw for next-generation, high-accuracy machine tools - NSK has developed a new type of ball screw that exhibits reduced motion errors to deliver higher surface finish quality for machine tools used in mould and die machining and other surface-critical applications.
Benefits of NSK NH series linear guides clearly visible in glass machining application
(2022-09-19)
Benefits of NSK NH series linear guides clearly visible in glass machining application - An Italian manufacturer of glass processing machinery is benefitting from the adoption of NH series linear guides from NSK.
NSK high-load ball screws now offer even longer life
(2022-07-25)
NSK high-load ball screws now offer even longer life - NSK has developed new technology that significantly extends ball screw life in high-load applications such as injection moulding machines and servo presses.
Packaging machine specialist standardises on NSK linear guides
(2022-07-04)
Packaging machine specialist standardises on NSK linear guides - Through Acumo, Österbergs Förpackningsmaskiner AB has now standardised on NSK linear guides, which offer quality, precision and long service life to users of its machines.
Timber plant reduces downtime with NSK linear guides
(2022-06-27)
Timber plant reduces downtime with NSK linear guides - Thanks to the adoption of NSK's linear guides with K1 lubrication units, a timber manufacturer managed to reduce conveyor downtime by a factor of more than 12, prompting annual cost savings of more than €77,000.
NSK roller guides increase uptime of blow moulding machines
(2022-05-16)
NSK roller guides increase uptime of blow moulding machines - A manufacturer of PET (polyethylene terephthalate) bottles frequently had to replace the linear guides on its blow moulding machines.
NSK’s NH/NS series linear guides benefit garment and textile printing machines
(2022-02-14)
NSK’s NH/NS series linear guides benefit garment and textile printing machines - A leading specialist in the development and manufacture of high-speed industrial digital printers for the garment, apparel and home textile industries, is benefiting from the many attributes of NH/NS series linear ...
Wave power – using NSK ball screws
(2021-12-06)
Wave power – using NSK ball screws: Swedish start-up company Ocean Harvesting is harnessing a new inexhaustible source of energy.
Linear Motion Control expands range of miniature linear components for medical equipment
(2021-10-04)
Expansion of miniature linear components for medical equipment - Human beings provide the measure: the drives of surgical robots, blood pumps, and MRI and CT equipment (for example), must offer a design that ensures they perform their tasks very precisely and smoothly without emitting any ...
Big performance from small NSK ball screws
(2021-09-13)
Big performance from small NSK ball screws - A new high-speed series of miniature large-lead ball screws from NSK Linear Motion Control offers a number of important benefits to users, including reduced product takt time, the potential to downsize equipment, and reduced power consumption.
Press brake specialist opts for NSK high-load ball screws
(2021-08-30)
Press brake specialist opts for NSK high-load ball screws: Following success with previous-generation machines, a leading manufacturer of press brakes is once again specifying high-quality NSK ball screws for its latest electric model.
Machining centers feature ball screws with nut cooling to increase surface quality of milled parts
(2021-08-16)
Machining centers feature ball screws with nut cooling to increase surface quality of milled parts - NSK ball screws with nut cooling are setting new standards in the precision of machine tools with mechanical drive components.
Machine tool builder benefits from NSK motion control solutions
(2021-07-12)
Machine tool builder benefits from NSK motion control solutions - Euromac, a global specialist in the design and manufacture of punching and bending machines, is benefitting from NSK ball screws, linear guides and bearings in two high-profile recent projects.
Monocarrier units in radiotherapy machines
(2021-07-05)
Monocarrier units in radiotherapy machines - A leading manufacturer of radiotherapy machines is using a Monocarrier linear drive unit from NSK to perform the precise movements and adjustments of the emitter, which projects the finely dosed X-rays or proton beams that kill cancer cells.
Automotive plant saves €577,000 a year by switching to NSK linear guides
(2021-06-28)
Automotive plant saves €577,000 a year by switching to NSK linear guides - After suffering an average of four linear guide failures a month on its process-critical component washing machines, a major automotive plant in Mexico is enjoying significant savings having switched to NH series linear ...
Share