Industrial Motors

Electric motors are used as the source of motive power in all kinds of industries.
NSK bearings are widely used in the revolving parts of motors. As well as enabling smooth and quiet rotation, they also perform a most important function by taking on the motor's load.
As the conservation of the environment rises up the global agenda, electricity is becoming more popular as a source of motive power, and customers have an increasing need for motors with low energy consumption. There is also demand for longer operational life, as a means of achieving even high reliability. In response to such demands, NSK delivers highly functional bearings that make full use of its core technologies: tribology.
These technologies —low energy consumption technologies and long operational life technologies — represent NSK's commitment to environmental protection, and the company will continue its activities in this field as one of its most important missions.
Share