Success Story
Industry: Electric Motors
Application: Electric motor with a frequency converter
Cost Savings: € 26 534
Introduction
The end customer produces viscose fibers for a wide variety of applications, such as sanitary materials or tea bags. In an electric motor with a frequency converter, the bearings had to be replaced 6 times a year due to electrical corrosion. NSK recommended the use of current-insulated deep groove ball bearings. After that, there were no more unplanned failures. This drastically reduced the costs associated with production downtime.
- Hygienic Papers - Viscose fibres
- Ceramic-Coated Insulated Ball Bearings HDY2
Key Facts
- The end customer produces viscose fibers for sanitary paper, tea bags and other applications
- The machine for the production of viscose fibers is driven by an electric motor with frequency converter
- Due to electrical corrosion, there were regular bearing failures. 6 times a year the bearings had to be replaced
- NSK reviewed the application and recommended the use of current-insulated deep groove ball bearings
- With HDY2C3 bearings the current permeability is reduced
- After the conversion to the NSK bearings, there were no more failures
Value Proposals
- The end customer produces viscose fibers for sanitary paper, tea bags and other applications
- The machine for the production of viscose fibers is driven by an electric motor with frequency converter
- Due to electrical corrosion, there were regular bearing failures. 6 times a year the bearings had to be replaced
- NSK reviewed the application and recommended the use of current-insulated deep groove ball bearings
- With HDY2C3 bearings the current permeability is reduced
- After the conversion to the NSK bearings, there were no more failures
Product Features
- The end customer produces viscose fibers for sanitary paper, tea bags and other applications
- The machine for the production of viscose fibers is driven by an electric motor with frequency converter
- Due to electrical corrosion, there were regular bearing failures. 6 times a year the bearings had to be replaced
- NSK reviewed the application and recommended the use of current-insulated deep groove ball bearings
- With HDY2C3 bearings the current permeability is reduced
- After the conversion to the NSK bearings, there were no more failures
Cost Saving Breakdown
Before | Cost p.a. | NSK Solution | Cost p.a. | |
---|---|---|---|---|
Bearing Costs | € 384 | Bearing Costs | € 410 | |
Engineering Costs | € 1 872 | Engineering Costs | € 312 | |
Costs of lost production | € 18 000 | Costs of lost production | € 500 | |
Lubrication Costs | € 50 | Lubrication Costs | € 50 | |
Other Costs | € 9 000 | Other Costs | € 1 500 | |
Total Costs | € 29 306 | € 2 772 |
Reference:SS-E-1-1048
Share