Mood, Industries, 1600x230

Introduction

A large OEM manufacturer of quarry and mining equipment used NSK products within their machinery. The nature of the application is very high vibration used to separate out product on a shaker screen. The bearing condition is very difficult to ascertain, so often they run to fail. These failures can incur loss of production and replacement part costs. NSK provided CMS service to analyse the condition of the bearing using our multi channel analyser which was able to distinguish between the machine natural vibration frequencies and the bearing frequencies, thus enabling NSK to determine the bearing health without stopping the machine.

 

Quarry, Mining, Construction, shaker screen, vibrating screen
  • Shaker Screen
  • NSK CMS Service

Key Facts

  • Bearing and motor details for the CMS analysis was as follows:
  • The shaker screen motor is rated at 12.5Kw
  • The shaker screen speed is adjustable, this ran at 1030 rpm
  • The combined bearing cartridge assembly was supplied with NSK spherical roller bearings
  • NSK Solution: Condition Monitoring Service (CMS) with detailed analysis to identify bearings and associated components health. NSK performed a full analyse of the shaker screen while it was in cycle
  • The CMS service indicated there were no concerns, the bearings were in good health

     

Value Proposals

  • An NSK expert performed an Condition Monitoring Service (CMS) on the running shaker screen
  • The test indicated there was no issue of concern from the bearings within the SX units
  • Regular monitoring of the bearing units will allow bearing health to be trended
  • 2 days to strip the shaker screen and investigate the potential bearing problem was avoided, along with the associated loss of production

     

Product Features

  • Live assessment of a machine's condition and health while the machine is still in operation
  • Predicted life of the critical components inside a machine allowing the customer to plan maintenance more accurately.

     

  • Early warning of problems occurring in machinery. Condition Monitoring is the most sensitive and long reaching method of detecting the signs of machine wear.
  • On-site support from NSK Engineers.
  • Assurance that NSK as a full range supplier can help with the provision of critical bearing and linear motion spares.

     

Cost Saving Breakdown
Before Cost p.a. NSK Solution Cost p.a.
Costs of lost production: 1 engineer to strip/refit the machine  € 800 Costs of lost production: No need for maintainance € 0
Engineering Costs: Machine runs for 10 hrs/day @800/hr production cost  € 16.000 Engineering Costs: No lost production cost € 0
Total Costs € 16 800 € 0

Reference:SS-E-2090