Mood, Industries, 1600x230

Introduction

Within NSK's own precision plant, a grinding machine was experiencing raceway form errors. After numerous attempts to correct the form error, the fault remains unidentified. Initial readings were taken using NSK Condition Monitoring Service prior to replacing the bearing. Subsequent, readings were taken within the following weeks. Results showed a number of issues associated with the spindle lubrication. This helped to identify the root cause of the machine problem and save time and costs on unnecessary investigative maintenance and machine downtime.

operator grinding mold and die part by universal grining machine
  • Spindle of Grinding Machine
  • Condition Monitoring Service (CMS)

Key Facts

  • Spindle of Grinding Machine
  • Grinding machine experiencing raceway form errors
  • NSK Solution: Condition Monitoring Service (CMS) with analysis on the spindle and dresser
  • Dresser: Gast air motor coupled to a belt drive delivering typical output speed of 8000 rpm
  • Spindle: Electric motor coupled to a belt drive delivering typical output speed of 17341 rpm
  • Root cause of the failures was identified
  • Time and cost saving realised

Value Proposals

  • NSK Condition Monitoring Service indicated there was a lubrication issue with the system subsequently leading to raised vibration levels from the rolling elements
  • The auto lubrication system on the machine was overhauled and the vibration levels reduced significantly
  • Three days to strip the spindle and investigate the potential bearing problem were avoided, along with the associated loss of production

Product Features

  • Live assessment of a machines condition and health while machine is still in operation
  • Predicted life of the critical components inside a machine allowing the customer to plan maintenance more accurately
  • Early warning of problems occurring in machinery. Condition Monitoring is the most sensitive and long reaching method of detecting the signs of machine wear
  • On-site support from NSK Engineers
  • Assurance that NSK as a full range supplier can help with the provision of critical bearing and linear motion spares
Cost Saving Breakdown
Before Cost p.a. NSK Solution Cost p.a.
Engineering Costs: Cost of maintenance € 4.050 Engineering Costs: No maintenance necessary € 0
Costs of lost production: Lost production cost € 7.250 Costs of lost production: No lost production time € 0
Total Costs € 11 300 € 0

Reference:SS-E-2080