Damage by Location

When analysing a bearing during periodic inspection of equipment, operating inspections or replacement of adjacent parts, the condition of the bearing should be determined.

The following points need to be considered when evaluating whether a bearing can be reused or not: abnormalities and damage located on the rolling surface (raceway / ball / roller), sliding surface (roller end / rib / flange / cage), outside surface, on the components (ring / ball / roller / cage), or on the entire bearing.

If the inspection discovers any damage which would prevent the bearing from being reused, then the bearing must be replaced with a new one.

 

Click a photo to visit page

Downloads