An Example of Environmentally Friendly Products

New Groove Shape Friction Plates contribute CO2 emission reduction by reducing the Friction Loss torque in the Automatic Transmission.

graph
New Groove Shape Friction Plates

New Groove Shape Friction Plates

New Groove Shape

New Groove Shape

In FY2020, 100 ktons*of COreduction is achieved.

*Calculated by the number of vehicles which have the new developed item application in the condition of 100,000 km running during 10 years.

~ai-d0c4c061-bfd5-4bc8-9c4a-ddc4c8a788d7_