Simulation Technology Development

Recently, CAE is a must process in product design and development to visualize invisible behavior helping to reduce development cost. NSK-Warner is developing such the CAE process in ourselves for further improvement of visualization and applying to product design.

MBD (Multi Body Dynamics) Simulation
Pawl-Type One-Way Clutch

Pawl-Type One-Way Clutch

MBD is a simulation method which can calculate the behavior of multiple components that interact with each other.

We can predict and validate the mechanical component behaviors by simulation without the need of real samples.

Structural Analysis
Shaft Clutch Assembly

Shaft Clutch Assembly

Structural analysis can calculate the stress/force and strain/deformation as the result of external and internal forces input.

Stress and deformation are generated in the products with complex shapes that can be calculated and simulated for the product improvements.

CFD (Computational Fluid Dynamics) Simulation
FP-Fluid flow simulation on Friction Paper

FP-Fluid flow simulation on Friction Paper

CFD can calculate the velocity and pressure of fluid flow. NSK-Warner products are being used in the AT(Automatic Transmission) and the environment is AT fluid/air mixed condition. The AT fluid and air flow in our products are calculated by the CFD simulation.